Skip to main content
Associate
March 24, 2026
Solved

stm32n6 usbd composite cdc+uvc failed to enumerate under windows

Hi,

The project was created in stm32mx from the example project cortexm_sysk.
It was generated as a CMake project and developed using VS Code.

The "USB Device Middleware Library MCU Software Component" library, version "V2.11.4 / 11-April-2025", was manually added.

CDC alone OK

UVC alone OK

CDC/HID OK

CDC/UVC NOT OK

See file in attachment.

I noticed the file descriptor is large (239 bytes). Is that a problem?

Is there another setting I need to change?

Regards,
Sébastien

FBLBest answer
ST Technical Moderator
September 3, 2026

Hi ​@sebastien.marion 

I assume the workaround proposed in this post might help you. If still having issue you can start a new discussion. 

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL

9 replies

ST Technical Moderator
March 30, 2026

Hi @sebastien.marion 

Based on your description, the behavior strongly points to an issue in the CDC + UVC configuration / class descriptors. To avoid guessing, the most helpful next step is a full descriptor dump of the failing CDC UVC configuration. If possible, provide USB trace using usb protocol analyzer.

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL
Associate
April 1, 2026

Hi @FBL 

Found in attachment wireshark capture of three configuration cdc only, uvc only, cdc+uvc.

I zip the prohect too, change define at the top of file usbd_conf.h to change configuration.

I see now enumerate cdc-uvc seem's right but only cdc is view by windows and functionnal, not the uvc.

 

regards,

Sébastien

ST Technical Moderator
April 2, 2026

Hi @sebastien.marion,

Thanks for sharing the traces and project.

From the USBPcap/Wireshark capture, the CDC+UVC configuration descriptor that Windows receives is structurally almost correct, but there is a descriptor inconsistency in the Video interface collection that explains why only CDC is exposed.

In your composite configuration: the UVC IAD correctly groups:

  • Interface 2: VideoControl (VC)
  • Interface 3: VideoStreaming (VS)

However, two fields still use interface numbers from the standalone UVC configuration (VC = 0, VS = 1):

  1. VideoControl header baInterfaceNr

    • bInCollection = 1
    • baInterfaceNr[0] = 1

    This value 1 is correct in a standalone UVC device (VS at interface 1), but in the composite build the VS interface is actually interface 3. So the VC header should point to interface 3, not 1.

  2. VideoStreaming alternate setting 1

    The descriptors show:

    • VS alt 0: interface 3, bAlternateSetting = 0, bNumEndpoints = 0 
    • VS alt 1: interface 1, bAlternateSetting = 1, bNumEndpoints = 1 

    For UVC, all alternate settings of the VideoStreaming interface must use the same interface number. In your composite, VS alt 1 should also be interface 3, not 1 (which is used by the CDC-Data interface).

Because of these mismatches (VC header pointing to 1, VS alt 1 declared as interface 1 while the IAD says the UVC function is on interfaces 2–3), the Windows UVC driver rejects the Video interface collection and does not bind to it. CDC remains valid, so only CDC is visible and functional.

The fix should be in the composite builder function USBD_CMPSIT_VIDEODesc():

  1. Use the dynamically assigned VS interface number in the VC header

    Replace the hard coded 1 with the actual VS interface index assigned by the composite builder:

    /* Class-specific VC Interface Header */
    pSVCInDesc->bInCollection = 0x01U;
    pSVCInDesc->baInterfaceNr = (uint8_t)pdev->tclasslist[pdev->classId].Ifs[1];

    Here:

    • Ifs[0] = VC interface number
    • Ifs[1] = VS interface number (shared by all VS alternate settings)
  2. Use the same VS interface number for the alt 1 interface descriptor

    Replace the hard coded interface number 1U:

    /* USB Standard VS Interface Descriptor - data transfer mode */
    /* Same interface as VS alt 0, Alternate Setting 1 */
    __USBD_CMPSIT_SET_IF(pdev->tclasslist[pdev->classId].Ifs[1],
     1U, /* AlternateSetting */
     1U, /* bNumEndpoints */
     UVC_CC_VIDEO,
     SC_VIDEOSTREAMING,
     PC_PROTOCOL_UNDEFINED,
     0U);

     

This ensures that VS alt 0 and VS alt 1 both use the same interface number 3.

After these two changes, the UVC IAD (interfaces 2–3), VC header, and VS descriptors all should be consistent.

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL
Associate
April 10, 2026

Hi,

Thank you for your answer.

I made the change, but unfortunately only the CDC is visible in the Windows Device Manager.

I've attached a Wireshark capture.
What checks can I perform?

regards,

Sébastien

ST Technical Moderator
April 13, 2026

Hi @sebastien.marion 

bAlternateSetting is still zero in frame 10 and 13 

FBL_0-1776079751024.png

FBL_1-1776080397009.png

I'm suspecting something missing in composite builder class. Let me check and get back to you.

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL
ST Technical Moderator
May 13, 2026

Hi @sebastien.marion 

Do you have any updates regarding this issue?

As a first step, I would suggest trying to register the Video class before the CDC ACM class, along with their corresponding interfaces descriptors.

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL
Associate II
June 23, 2026

Hi,

I'm encountering the same issue on the STM32N657X0-NUCLEO board using USBX (Azure RTOS).

Configuration

  • STM32N657X0
  • USB OTG HS (embedded PHY)
  • USBX middleware
  • Composite device: Dual CDC ACM + UVC Video

Current Status

A dual CDC ACM device enumerates correctly, and both /dev/ttyACM* interfaces appear on the Linux host.

However, as soon as I add the UVC Video class, USB enumeration fails completely. The host does not detect the device, and no entry appears in lsusb.

What I've Already Tried

  • Added FIFO allocation for the UVC isochronous endpoint:
HAL_PCDEx_SetRxFiFo(&hpcd, 512);
HAL_PCDEx_SetTxFiFo(&hpcd, 7, 1024);
  • Changed the Video endpoint address from 0x81 to 0x87 to avoid conflicts with the CDC endpoints.
  • Corrected the aInterfaceNr field in the Video Control Header descriptor (CubeMX generates 0x01, but the correct Video Streaming interface is 0x05 in my composite configuration).
  • Increased USBX resource limits:
#define UX_MAX_DEVICE_ENDPOINTS   8
#define UX_MAX_DEVICE_INTERFACES 8
  • Disabled incomplete isochronous transfer interrupts:
USB1_OTG_HS->GINTMSK &=
~(USB_OTG_GINTMSK_IISOIXFRM |
USB_OTG_GINTMSK_PXFRM_IISOOXFRM);

Unfortunately, none of these changes resolved the issue.

Were you able to find a solution? Also, is there a known working CDC + UVC composite device example for STM32N6 using USBX?

Associate
May 15, 2026

Hi,

Unfortunately I could not test it immediately as I am no longer part of the project with this need.

Thank you for your feedback.

Regards,

Sébastien

FBLBest answer
ST Technical Moderator
September 3, 2026

Hi ​@sebastien.marion 

I assume the workaround proposed in this post might help you. If still having issue you can start a new discussion. 

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL