Skip to main content
Associate II
August 29, 2025
Question

STM32N6 JPEG Encoder HAL Driver Not Supporting RGB from Datasheet

I'm developing camera-related things on the N6, and while perusing the JPEG encoder, I noticed that the datsheet and registers for it seem to indicate it can convert raw RGB (565? 888?) to JPEG. This is alongside Grayscale, YUV, and CMYK. However, in the HAL driver, there only seem to be defines and code around the last three. There are defines and support for Greyscale, YCbCr (which I assume to be YUV from the datasheet? But that is also confusing), and for CMYK. But there is little to no reference at all of the RGB options in the JPEG encoder. Is this functionality not supported? Am I missing something? Is it a bug in the firmware? 

While I'm on the subject, am I able to pump the YUV420 planar from the DCMIPP into the JPEG Encoder? The datasheet suggests I can but all examples and information I canf ind online suggests I need to convert it to YCbCr first, but I thought they were the same?

Thanks for Support

This topic has been closed for replies.

1 reply

Lina_DABASINSKAITE
ST Community Manager
August 29, 2025

Hello @chornbeck,

Your message is escalated to the Online support team. They will reach out to you directly. 

Regards,
Lina

​In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.