Skip to main content
Associate II
Feb 24, 2026 6:18 PM UTC
Question

STM32N6 – HardFault (INVPC) when calling tx_thread_schedule() in Non-Secure

Hi everyone,

I’m working on an STM32N6 project configured with:

  • ThreadX running in Non-Secure

  • SAU configured

  • RISAF configured

  • External Memory Manager enabled(Load and Run mode)

The project is very simple. However, when debugging the Non-Secure application, as soon as tx_thread_schedule() is called, execution jumps to HardFault.
The Fault Analyzer reports: “Attempt to do exception with bad value in EXEC_RETURN number (INVPC)”.

The code is loaded in external flash memory using Load and Run mode, the signed bin files are uploaded in the external flash using STM32CubeProg and then debugged using STM32CubeIDE.
Has anyone experienced INVPC errors on STM32N6 with ThreadX in Non-Secure?
Any suggestions would be greatly appreciated.

1 reply

ST Technical Moderator
Mar 24, 2026 2:35 PM UTC

Hello @LisaB 

Please refer to the article below to debug your HardFauld.

How to debug a HardFault on an Arm® Cortex®-M STM3... - STMicroelectronics Community

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om