Skip to main content
svogl
Associate III
April 1, 2026
Solved

stm32n6 gpio interrupts: exti irqhandler missing

Dear all,

I have been modifying the VENC_SDCard_ThreadX example and wanted to start some activity based on the user button, triggered by interrupt using the usual HAL + BSP helpers to init the gpio, and registering a handler function for falling flanks.

So I tried

	BSP_PB_Init(BUTTON_USER1, BUTTON_MODE_EXTI);

and implemented BSP_PB_Callback(). 

Symptom: Hitting the button turned the program to be stuck in some unrelated irqhandler (debugger name-clash -- the defaulthandler triggered), the callback has not been triggered.

I had a look at the BSP implementationn and retried the same with HAL functions, same effect, this code in BSP_PB_Init() sparked my interest:

 (void)HAL_EXTI_GetHandle(&hpb_exti[Button], BUTTON_EXTI_LINE[Button]);
 (void)HAL_EXTI_RegisterCallback(&hpb_exti[Button], HAL_EXTI_COMMON_CB_ID, ButtonCallback[Button]);

which registers a callback,  and further down the line in stm32n6xx-hal-driver-exti.c there is an HAL_EXTI_IRQHandler  implementation which is not called.

Long story short, the example code seems to miss init code for the actual EXTIxx_IRQHandler. 

// GPIO C13 USER button / exti channel 13
void EXTI13_IRQHandler(void) {
 HAL_EXTI_ClearPending(&hpb_exti_user, EXTI_TRIGGER_FALLING);

 btnCallback(); // in my code I simply perform the action needed not going through HAL
}

the IRQ handler needs a reference to the exti configuration, which the BSP code initialized:

static EXTI_HandleTypeDef hpb_exti_user;

//... near the top of main(), after calling BSP_PB_Init():
	HAL_EXTI_GetHandle(&hpb_exti_user, EXTI_LINE_13); // USER

I had a look at a fresh CubeMX project, and seemingly the EXTI...IRQHandler functions are not generated.

This code works, but it is a hack - did I miss some code generator option for EXTI? 

Thanks for some insights

Simon

 

 

ANJSBest answer
ST Employee
April 1, 2026

Hello!
Have you checked the NVIC enabled in the GPIO config to generate interrupt?
Best regards
ANJS

 

2 replies

ANJSBest answer
ST Employee
April 1, 2026

Hello!
Have you checked the NVIC enabled in the GPIO config to generate interrupt?
Best regards
ANJS

 
svogl
svoglAuthor
Associate III
April 1, 2026

Ahhh, THERE it is, thanks :)