Skip to main content
Visitor II
Sep 10, 2026 6:42 AM UTC
Question

STM32N6 DCMIPP: NNPipe works in continuous mode but not in snapshot mode

I’m trying to run a fork of the STM32N6-GettingStarted-ObjectDetection project for the STM32N6570-DK on my own board.

My board has the same clock configuration, memory interface, and LCD interface as the STM32N6570-DK. However, instead of a CSI camera, I’m using an 8-bit parallel camera interface.

The frames come from a custom FPGA source with the following parameters:

  • 75 MHz clock at 8 bit width bus
  • YUV422
  • 1280 × 768
  • 30 fps
  • Embedded synchronization ITU656

My changes to the original project are:

  • Added GPIO initialization for the 8-bit parallel camera interface.
  • Changed the DCMIPP configuration from CSI to parallel mode:
const DCMIPP_EmbeddedSyncCodesTypeDef syncСodes = {
.FrameStartCode = 0xAB, /* frame SAV*/
.LineStartCode = 0x80, /* line SAV */
.LineEndCode = 0x9D, /* frame EAV */
.FrameEndCode = 0xB6 /* line EAV */
};

const DCMIPP_ParallelConfTypeDef pParallelConfig = {
.Format = DCMIPP_FORMAT_YUV422,
.VSPolarity = DCMIPP_VSPOLARITY_LOW,
.HSPolarity = DCMIPP_HSPOLARITY_LOW,
.PCKPolarity = DCMIPP_PCKPOLARITY_RISING,
.ExtendedDataMode = DCMIPP_INTERFACE_8BITS,
.SynchroMode = DCMIPP_SYNCHRO_EMBEDDED,
.SynchroCodes = syncСodes,
.SwapBits = DCMIPP_SWAPBITS_DISABLE,
.SwapCycles = DCMIPP_SWAPCYCLES_ENABLE
};

/* Set parallel mode */
ret = HAL_DCMIPP_PARALLEL_SetConfig(&hcamera_dcmipp, &pParallelConfig);
assert(ret == HAL_OK);
  • Using 
    HAL_DCMIPP_PIPE_Start(&hcamera_dcmipp, pipe, (uint32_t)pbuff, mode);

    instead of

    HAL_DCMIPP_CSI_PIPE_Start(&hcamera_dcmipp, pipe, DCMIPP_VIRTUAL_CHANNEL0, (uint32_t)pbuff, mode);

    for pipe start

  • Commented out the CSI clock configuration.
  • Added YUV-to-RGB conversion to the ISP:
DCMIPP_ColorConversionConfTypeDef yuv_conv_config = {0};

yuv_conv_config.ClampOutputSamples = ENABLE;
yuv_conv_config.OutputSamplesType = DCMIPP_CLAMP_RGB;

yuv_conv_config.RR = 409;
yuv_conv_config.RG = 298;
yuv_conv_config.RB = 0;
yuv_conv_config.RA = -223;

yuv_conv_config.GR = -208;
yuv_conv_config.GG = 298;
yuv_conv_config.GB = -100;
yuv_conv_config.GA = 135;

yuv_conv_config.BR = 0;
yuv_conv_config.BG = 598;
yuv_conv_config.BB = 517;
yuv_conv_config.BA = -277;

ret = HAL_DCMIPP_PIPE_SetYUVConversionConfig(
&hcamera_dcmipp,
DCMIPP_PIPE1,
&yuv_conv_config);

if (ret != HAL_OK)
{
return CMW_ERROR_PERIPH_FAILURE;
}

ret = HAL_DCMIPP_PIPE_EnableYUVConversion(
&hcamera_dcmipp,
DCMIPP_PIPE1);

if (ret != HAL_OK)
{
return CMW_ERROR_PERIPH_FAILURE;
}

With these changes, I can successfully display the video on the LCD after starting:

CameraPipeline_DisplayPipe_Start(lcd_bg_buffer, CMW_MODE_CONTINUOUS);

So the DCMIPP configuration seems to be working correctly, at least in continuous display mode.

However, I have a problem with the NNPipe.

When I run:

CameraPipeline_NNPipe_Start(nn_in, CMW_MODE_SNAPSHOT);

while (cameraFrameReceived == 0) {};
cameraFrameReceived = 0;

SCB_InvalidateDCache_by_Addr(nn_in, nn_in_len); // debug

inside the main loop, cameraFrameReceived becomes 1, so the frame-received callback appears to be triggered.

However, when I inspect the nn_in buffer, only the first 4 bytes have changed to 0x00FFFFFF. The rest of the buffer contains stale/garbage data and does not change between frames.

Interestingly, if I start the NNPipe in continuous mode before entering the main loop:

CameraPipeline_NNPipe_Start(nn_in, CMW_MODE_CONTINUOUS);

and commented out this section inside main loop:

//CameraPipeline_NNPipe_Start(nn_in, CMW_MODE_SNAPSHOT);

I get valid frames in the nn_in buffer. I can export the buffer contents from the memory browser, convert them to BMP, and the resulting image looks correct.

So the DCMIPP/ISP pipeline appears to capture and process the frames correctly in continuous mode, but the same pipeline does not seem to update the buffer correctly in snapshot mode.

What am I missing?

Could this be related to:

  • DCMIPP Pipe configuration?
  • DMA/cache coherency?
  • Сlock configuration?
  • The difference between CMW_MODE_CONTINUOUS and CMW_MODE_SNAPSHOT?
  • Some required reconfiguration or restart of the NNPipe between snapshots?

Any suggestions on where to look would be greatly appreciated.

1 reply

KDJEM.1
ST Technical Moderator
Sep 17, 2026 10:15 AM UTC

Hello ​@Sergey Burenkov and welcome to the community;

 

I recommend you to start with an available example like as DCMIPP_SnapshotDecimationMode and get inspired to develop your own application.

This example shows how to use the DCMIPP IP in Snapshot Mode as a Camera Serial Interface and it is based on the STM32Cube HAL API that can be used to build any firmware application. 

 

I hope this help you.

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.