Skip to main content
Associate II
Mar 20, 2024 5:32 AM UTC
Solved

STM32L4S5VIT6 with AWS

Hi,

    Good morning, everyone. I'm new to IOT. So, I need your help for how to connect and use STM32L4S5VIT6 and AWS from the scratch. Could you please help me. Demo video or any sample code and share any related document for understanding purpose it is very helpful for us.

This topic has been closed for replies.
STTwo-32
STTwo-32Best answer
ST Technical Moderator
Mar 22, 2024 8:41 AM UTC

All available examples are included on the version 3.0.0 of the X-CUBE-AWS (but without .ioc files).

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

10 replies

STTwo-32
ST Technical Moderator
Mar 20, 2024 8:12 AM UTC

Hello @M_Sukumar 

I suggest you to use the examples of the X-CUBE-AWS (version 2.2.0 not the last version). If you want to use the last version, you should switch to the B-U585I-IOT02A.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
M_SukumarAuthor
Associate II
Mar 20, 2024 8:59 AM UTC

Hi STTwo-32,

    if I need to create from scratch. do you have any documents?

STTwo-32
ST Technical Moderator
Mar 20, 2024 9:22 AM UTC

You can refer to one of the examples on the X-Cube to start your project. Then, do the necessary modification to be compatible with your needs.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
M_SukumarAuthor
Associate II
Mar 21, 2024 4:45 AM UTC

Hi STTwo-32,

          .ioc file is not there how can integrate that file.

STTwo-32
ST Technical Moderator
Mar 21, 2024 5:34 AM UTC

The examples on this X-Cube are generated without using CubeMX. So, there is no .ioc file. If you want to use a .ioc file, you need to create it from scratch.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
M_SukumarAuthor
Associate II
Mar 21, 2024 5:57 AM UTC

Hi STTwo-32,

      yeah, I need to create from scratch. Could you please help from that. Do you have any documents related to STM32l4 to AWS from Scratch.

STTwo-32
ST Technical Moderator
Mar 21, 2024 6:39 AM UTC

The best suggestion that I can give you now is to understand how this examples Work and try to reproduce them using CubeMX and adapt them to your needs.

Best Regrads.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
M_SukumarAuthor
Associate II
Mar 22, 2024 6:30 AM UTC

Hi STTwo-32,

    Could you please share any example for B-U585I-IOT02A control board to directly communicate with the AWS s3 bucket. 

Best Regard,

Sukumar.M

STTwo-32
STTwo-32Best answer
ST Technical Moderator
Mar 22, 2024 8:41 AM UTC

All available examples are included on the version 3.0.0 of the X-CUBE-AWS (but without .ioc files).

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.