Skip to main content
Associate
Jan 28, 2026 3:23 AM UTC
Question

STM32L475RCT6 Flash Erase Error

I'll explain Flash Erase Error to the stm32l475rct6 MCU that I'm currently using. Page : 127, Address : 0x0803F800, Bank : FLASH_BANK_1 is defined, and if you try to modify the value after first saving the value in the Flash area, the values already stored in Flash are not erased properly, so the Flash value cannot be modified. SMT32CubeIDE version is 1.19.0 and I'll attach the code I implement, so please check where the problem is and let me know if there is a solution.

void AO_SaveCalibration(void)

{

HAL_StatusTypeDef status;

 

printf("Saving calibration to Flash...\r\n");

printf("Data size: %u bytes\r\n", sizeof(AO_Calibration_t));

 

ao_cal.checksum = Calculate_Checksum1();

 

status = HAL_FLASH_Unlock();

 

if (status != HAL_OK)

{

printf("ERROR: Flash unlock failed\r\n");

return;

}

 

__HAL_FLASH_CLEAR_FLAG(FLASH_FLAG_ALL_ERRORS);

 

while(__HAL_FLASH_GET_FLAG(FLASH_FLAG_BSY))

{

// Flash 작업 완료 대기

}

 

FLASH_EraseInitTypeDef EraseInitStruct;

uint32_t PageError = 0;

EraseInitStruct.TypeErase = FLASH_TYPEERASE_PAGES;

EraseInitStruct.Banks = FLASH_BANK_1;

EraseInitStruct.Page = CAL_FLASH_PAGE;

EraseInitStruct.NbPages = 1;

 

status = HAL_FLASHEx_Erase(&EraseInitStruct, &PageError);

if (status != HAL_OK)

{

printf("ERROR: Flash erase failed! Status=0x%02X, PageError=0x%08lX\r\n",

status, PageError);

HAL_FLASH_Lock();

return;

}

 

while(__HAL_FLASH_GET_FLAG(FLASH_FLAG_BSY))

{

// Erase 작업 완료 대기

}

 

uint64_t *data_ptr = (uint64_t*)&ao_cal;

uint32_t data_size = sizeof(AO_Calibration_t);

uint32_t num_doublewords = (data_size + 7) / 8;

uint32_t write_addr = CAL_FLASH_ADDR;

 

printf("Writing %lu doublewords to Flash...\r\n", num_doublewords);

 

for (uint32_t i = 0; i < num_doublewords; i++)

{

status = HAL_FLASH_Program(FLASH_TYPEPROGRAM_DOUBLEWORD,

write_addr,

data_ptr[i]);

 

if (status != HAL_OK)

{

printf("ERROR: Flash write failed at 0x%08lX (status: 0x%02X)\r\n",

write_addr, status);

printf(" Flash error code: 0x%08lX\r\n", HAL_FLASH_GetError());

 

HAL_FLASH_Lock();

return;

}

 

write_addr += 8;

}

 

HAL_FLASH_Lock();

 

printf("Calibration saved! (Checksum: 0x%08lX)\r\n", ao_cal.checksum);

 

// 저장된 내용 확인

printf("\r\n=== Saved Data ===\r\n");

for (int ch = 0; ch < AO_CH_MAX; ch++)

{

printf(" %s: 4mA=%u, 20mA=%u, Sensor=%s, EN=%s\r\n",

AO_GetChannelName(ch),

ao_cal.channels[ch].pwm_4mA,

ao_cal.channels[ch].pwm_20mA,

AO_GetSensorTypeName((Sensor_Type_t)ao_cal.channels[ch].sensor_type),

ao_cal.channels[ch].enabled ? "Yes" : "No");

}

printf("==================\r\n\r\n");

}

3 replies

TDK
Jan 28, 2026 4:25 AM UTC

What does the printf story tell when you try to run this code? What error messages does it present?

"If you feel a post has answered your question, please click ""Accept as Solution""."
Associate
Jan 28, 2026 4:46 AM UTC

- Programming Alignment Error (FLASH_SR_PGAERR)
- Programming Sequence Error (FLASH_SR_PGSERR)
- Programming Parallelism Error (FLASH_SR_PROGERR)

 

 

TDK
Jan 28, 2026 11:47 AM UTC

What gets printed out through printf when you run the code and the error happens? Show the log.

"If you feel a post has answered your question, please click ""Accept as Solution""."