Skip to main content
Associate II
Aug 20, 2025 4:13 PM UTC
Question

stm32l452 timer interrupt and can tle9255w

Hello, 

I am starting a timer interrupt to send data over can data at 50 ms below is the configuration for the same and callback function when pulse is complete

volatile uint8_t send_ch0_flag = 0;

volatile uint8_t send_chx_flag = 0;

volatile uint8_t send_relay_flag = 0;

void MX_TIM2_Init(void)

{

TIM_ClockConfigTypeDef sClockSourceConfig = {0};

TIM_MasterConfigTypeDef sMasterConfig = {0};



htim2.Instance = TIM2; 

htim2.Init.Prescaler = 3999; // 80 MHz / (3999+1) = 20 kHz 

htim2.Init.CounterMode = TIM_COUNTERMODE_UP; 

htim2.Init.Period = 999; // (999+1) / 20kHz = 0.05 s = 50 ms 

htim2.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1; 

htim2.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE; 

__HAL_RCC_TIM2_CLK_ENABLE();

if (HAL_TIM_Base_Init(&htim2) != HAL_OK) 

{ 

 Error_Handler(); 

} 



sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL; 

if (HAL_TIM_ConfigClockSource(&htim2, &sClockSourceConfig) != HAL_OK) 

{ 

 Error_Handler(); 

} 



sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET; 

sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE; 

if (HAL_TIMEx_MasterConfigSynchronization(&htim2, &sMasterConfig) != HAL_OK) 

{ 

 Error_Handler(); 

} 



HAL_NVIC_SetPriority(TIM2_IRQn, 1, 0); 

HAL_NVIC_EnableIRQ(TIM2_IRQn); 



HAL_TIM_Base_Start_IT(&htim2);



}

void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim)

{

 if (htim->Instance == TIM2) 

 {

 ms_counter += 50;



 // Channel 0 every 50 ms

 send_ch0_flag = 1;



 // Channels 1–8 every 100 ms

 if (ms_counter % 100 == 0) {

 send_chx_flag = 1;

 }



 // Relay every 1000 ms

 if (ms_counter % 1000 == 0) {

 send_relay_flag = 1;

 ms_counter = 0; // reset counter

 }

 }

}

void process_CAN_messages(void) //called inside while loop

{

 if (send_ch0_flag) {

 send_ch0_flag = 0;

 CAN_SendChannel(0); // your wrapper function

 }



 if (send_chx_flag) {

 send_chx_flag = 0;

 for (int ch = 1; ch < 9; ch++) {

 CAN_SendChannel(ch);

 }

 }



 if (send_relay_flag) {

 send_relay_flag = 0;

 sendRelayMessages();

 }

}

Please let me know what configuration I am doing wrong or is it a code issue.

But when I send a command over can to the mcu I am not able to recieve the command but the same is working when I am starting the timer at 100ms. Below is the can reception logic. The CAN transrx ic i am using is TLE9255W.

Inside while I am monitoring my can transrx interrupt below is the interrupt

void HAL_CAN_RxFifo0MsgPendingCallback(CAN_HandleTypeDef *hcan){

HAL_CAN_GetRxMessage(&hcan1, CAN_RX_FIFO0, &RxHeader, RxData);

if(RxHeader.DLC == 8){

data_received = 1; //monitored inside while loop

}

}

Thanks

 

This topic has been closed for replies.

6 replies

mƎALLEm
ST Technical Moderator
Aug 21, 2025 7:49 AM UTC

Hello,

I'm not sure I understood the issue. Please elaborate more that statement: 


@yashg25 wrote:

But when I send a command over can to the mcu I am not able to recieve the command but the same is working when I am starting the timer at 100ms. Below is the can reception logic. The CAN transrx ic i am using is TLE9255W.


 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
yashg25Author
Associate II
Aug 21, 2025 8:09 AM UTC

Hello @mƎALLEm ,

What I meant by that statement is that :
Statement 1:

When I set the timer period to generate interrupt at every 50ms (for sending data from stm32l452re to CAN device which is working but on my CAN device I see the reception time around 90ms even for a 50ms interrupt),
I am not able to send the can command from my CAN device to stm32l452re CAN, the command is not executing.

 

Statement 2:

But when I set the timer period to generate interrupt at every 100ms(for sending data from stm32l452re to CAN device which is working and on my CAN device I see the reception time around 100ms),

I am able to send the can commands from my CAN device to stm32l452re CAN, the command that I am sending are executing.


Thanks,
Yash

yashg25Author
Associate II
Aug 22, 2025 4:09 AM UTC

@mƎALLEm , Waiting for your reply.

ST Employee
Aug 25, 2025 10:30 AM UTC

Hi @yashg25, 

Since CAN communication fails when the timer interrupt is set to 50 ms but works at 100 ms, this is likely due to interrupt timing conflicts or priority mismanagement; the timer interrupt can be preempting the CAN interrupt, can you share interrupt priorities? 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
yashg25Author
Associate II
Aug 26, 2025 12:26 PM UTC

Hello @Sarra.S,

Below are the priorities :

1. Timer interrupt

HAL_NVIC_SetPriority(TIM2_IRQn, 1, 0);

HAL_NVIC_EnableIRQ(TIM2_IRQn);

2. CAN interrupt

HAL_NVIC_SetPriority(CAN1_RX0_IRQn, 0, 0);

HAL_NVIC_EnableIRQ(CAN1_RX0_IRQn);

Regards,

Yash Gupta

 

Karl Yamashita
Principal
Aug 26, 2025 6:47 PM UTC

You're not showing enough code. 

What is going on in CAN_SendChannel and sendRelayMessages? 

 

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.CAN Jammer an open source CAN bus hacking toolCANableV3 Open Source