Skip to main content
RKnoe
Associate
Jun 21, 2019 1:44 PM UTC
Question

STM32L412 hardfault while using minimal CubeIDE example.

I try to set up an USB CDC project for a STM32L412KB Nucleo32 board using CubeIDE.

I activated the USB connection and the USB middleware with the default USB CDC setup.

If I run this code, it ends in the hardfault handler with INVSTATE raised during the USB_EnableGlobalInt(hpcd) call (HAL_PCD_Start() at stm32l4xx_hal_pcd.c:1,014 0x8000d26).

The next items on the call stacks are: <signal handler called>() at 0xfffffff9, 0x0, <signal handler called>() at 0xfffffff1   and finally HardFault_Handler() at stm32l4xx_it.c:88 0x800432a.

Currently I ran out of ideas on what to do. USB CDC worked in projects set up for the STM32F072 and F103 - should we change from the L4 to another MCU?

This topic has been closed for replies.

20 replies

waclawek.jan
Super User
Jul 21, 2019 11:19 PM UTC

> thanks for the hint Jan, but when I do singel step, it works fine until I push resume.

> So I can single step trough the whole thing and it is fine, but when I let the processor run freely again it ends up in HardFault.

My guess is, that the problem occurs in the USB interrupt service routine (ISR), and you have disabled interrupts during single-step (that's a common setting, otherwise it would be hard to single-step most practical programs).

You may perhaps want to place a breakpoint into the USB ISR and single-step from there to see, where that will take you.

Do you have a PC connected to the USB when the problem occurs?

JW

Tesla DeLorean
Guru
Jul 22, 2019 12:26 AM UTC

Should check for malloc()/free() idiocy that they like to do in interrupt context

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
lizerd
Associate III
Jul 22, 2019 9:54 AM UTC

YESSSSS.

ruediger1.561124119260664E12 Hade the right answer to my problem.

Missing IRQ routine linkage .

@RKnoe​ Thanks

ruediger1.561124119260664E12
 
(Community Member)
2 hours ago
 
Yes. For me the reason was a forgotten ISR definition in the Startup/startup_stm32l412kbux.s file. It should contain:
 
 
 
 .word 0
 
 .word COMP_IRQHandler
 
 .word LPTIM1_IRQHandler
 
 .word LPTIM2_IRQHandler
 
 .word USB_IRQHandler
 
 .word DMA2_Channel6_IRQHandler
 
 .word DMA2_Channel7_IRQHandler

waclawek.jan
Super User
Jul 22, 2019 1:30 PM UTC

The USB_IRQHandler vector is present in both arm and iar version of startup code, absent only in the gcc version. IMO it's a bug. @Imen DAHMEN​  can you please have a look? Thanks.

JW

ST Technical Moderator
Aug 15, 2019 8:47 AM UTC

Hello All,

This issue is raised internally for fix.

Thanks for your contribution.

Best Regards,

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks