Skip to main content
angeletti2
Associate III
December 20, 2017
Question

STM32L4 wake up from STOP2, setting core clock to 80MHz

  • December 20, 2017
  • 1 reply
  • 815 views
Posted on December 20, 2017 at 13:52

Good afternoon everyone,

I'm working on a ultra low power FreeRTOS application, in which I need to enter and exit continously the STOP2 mode from my MCU, STM32L476RG. The problem is that I need to wake up working at 80MHz. My implementation works pretty much everytime, but sometimes it hangs within the function (attached) that sets the core clock to MSI with PLL at 80MHz. Anyone knows why it happens? In the specific, it hangs during the check of 'HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK'

Regards,

Fabio 

#freertos #low-power #stm32l4 #stop2 #lowpower-sleep
This topic has been closed for replies.

1 reply

dtarrago
Associate III
January 29, 2018
Posted on January 29, 2018 at 10:00

Hi Fabio,

Did you solve that? I'm facing similar behaviour: my application could be perfectly working and, after maybe two days, it stops working at same function 'H

AL_RCC_OscConfig' when waking up from Stop2 mode

....

Best regards,

Dani.