Skip to main content
SThom.7
Associate III
Dec 15, 2025 12:49 PM UTC
Solved

STM32L4 updated HAL drivers breaks HAL_UARTEx_ReceiveToIdle_DMA

I have updated the STM32L4 HAL drivers to V1.13.6 / 14-November-2025 (1.18.2), which has broken my implementation of HAL_UARTEx_ReceiveToIdle_DMA.

Is this a fault in the new HAL drivers or does user code need to be updated inside the HAL_UARTEx_RxEventCallback?

SThom.7
SThom.7Best answer
Associate III
Jan 8, 2026 5:55 AM UTC

5 replies

TDK
Dec 15, 2025 12:58 PM UTC

Code within HAL_UARTEx_ReceiveToIdle_DMA hasn't changed for several years. Probably not the problem.

https://github.com/STMicroelectronics/stm32l4xx-hal-driver/blame/047a8610c7dc0dcfdb4cd63b86cd3a2cbd3e5899/Src/stm32l4xx_hal_uart_ex.c#L945

 

Debug your code. Hit pause, understand what is breaking and then try to fix that. Don't look for a magic solution.

Do a diff on your code before/after the update to understand the differences. CMSIS and header files need to be in sync with HAL files.

"If you feel a post has answered your question, please click ""Accept as Solution""."
SThom.7
SThom.7Author
Associate III
Dec 15, 2025 1:03 PM UTC

Diff shows the code around this feature has definitely been updated in hal_uart.c

Release notes:

  • Provide accurate position in RxEventCallback when ReceptionToIdle mode is used with DMA, when UART and DMA interrupts process is delayed."
SThom.7
SThom.7Author
Associate III
Dec 17, 2025 2:32 PM UTC

I have found the fault in stm32l4xx_hal_uart.c

Inside the function UART_DMAReceiveCplt, inside the check for HAL_UART_RECEPTION_TOIDLE line 3902, this line of code is missing.

huart->RxXferCount = 0;

ST Technical Moderator
Dec 24, 2025 4:19 PM UTC

Hello @SThom.7 

Could you share your code please?

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om
SThom.7
SThom.7AuthorBest answer
Associate III
Jan 8, 2026 5:55 AM UTC