Skip to main content
MLy
Associate II
September 6, 2018
Question

STM32L152 HAL libary - USART, - no TX transmission ?

  • September 6, 2018
  • 0 replies
  • 371 views

Dear Sir,

Now I am using HAL library ( STM32Cube_FW_L1_V1.8.0)

after setup USART 3, and

after running, in some case, I need to disable the transmit interrupt by using

__HAL_UART_DISABLE_IT(&UartHandle, UART_IT_TXE);

But then if I need to re-transmit some data from buffer, even using

HAL_UART_Transmit_IT(&UartHandle, (uint8_t*)aTxBuffer, TXBUFFERSIZE);

It will not transmit out any data nor having any USART interrupt.

Thanks!

Martin

This topic has been closed for replies.