Skip to main content
Associate II
April 21, 2026
Question

STM32H7S78-DK: USBX PIMA / MTP is not supported in standalone mode

Dear community members,

STM32H7S78-DK: USBX standalone (CDC ACM + PIMA) works in HS now but PIMA / MTP is not supported in standalone mode in USBX

Currently, it is not possible to use the PIMA/MTP class in USBX in standalone mode (without an RTOS). The MTP implementation depends on Azure RTOS ThreadX, and there is no official support for running it in bare-metal configurations.

When attempting to use it in standalone mode, the stack returns:

#define UX_FUNCTION_NOT_SUPPORTED 0x54

This is also reflected in the official documentation:

USBX Getting Started – Bare-metal support matrices 

1 reply

ST Technical Moderator
April 22, 2026

Hello @polEscudero 

Indeed, USBX PIMA /MTP is not supported in standalone mode in current STM32CubeH7RS. It is planned to be supported in STM32CubeC5. 

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL