Skip to main content
Associate
September 23, 2026
Solved

STM32H7RS HAL: IS_SPI_LIMITED_DATASIZE rejects 9-bit on SPI4/SPI5, but RM0477 says 4–16 bits are supported

  • September 23, 2026
  • 3 replies
  • 65 views

Hello,

I am using an STM32H7S3 with STM32CubeH7RS HAL [V1.2.1]. SPI5 drives a display over 3-wire SPI with 9-bit frames (the 9th bit carries D/C).

With USE_FULL_ASSERT enabled, HAL_SPI_Init() triggers an assert in stm32h7rsxx_hal_spi.c (line 259 in the current GitHub version):

if (IS_SPI_LIMITED_INSTANCE(hspi->Instance))
{
  assert_param(IS_SPI_LIMITED_DATASIZE(hspi->Init.DataSize));
  assert_param(IS_SPI_LIMITED_FIFOTHRESHOLD(hspi->Init.FifoThreshold));
}

In stm32h7rsxx_hal_spi.h, the macro only accepts 8-bit and 16-bit:

#define IS_SPI_LIMITED_DATASIZE(DATASIZE)  (((DATASIZE) == SPI_DATASIZE_16BIT) || \
                                            ((DATASIZE) == SPI_DATASIZE_8BIT))

However:

1. RM0477 [rev 10], section 55.3, Table 578 states that for SPI4 and SPI5 the data and CRC size is "configurable from 4 to 16 bits".

2. The HAL itself is inconsistent. A few lines below the assert, the runtime check in HAL_SPI_Init() only rejects sizes above 16 bits for limited instances:

if ((IS_SPI_LIMITED_INSTANCE(hspi->Instance)) && (hspi->Init.DataSize > SPI_DATASIZE_16BIT))
{
  return HAL_ERROR;
}

3. In practice, init succeeds with SPI_DATASIZE_9BIT and the display works correctly. [Optional: A logic analyzer capture shows 9 SCK pulses per frame.]

For comparison, the same macro in the STM32U5 and STM32H5 HAL also accepts only 8/16 bits, which matches RM0456 (DSIZE[2:0] reserved on limited instances). The STM32N6 HAL accepts the full 4–16 bit range. It looks like the H7RS macro was carried over from U5/H5, while the H7RS hardware behaves differently.

Small side note on Table 578: the SPI4/SPI5 column header also says "full-featured instances", although the values in that column are clearly the limited ones. The FIFO threshold row says 1–16 data for an 8x8-bit FIFO, while the HAL limits it to 8 data and checks the packet size against 8 bytes.

Questions:
- Can ST confirm that SPI4/SPI5 on STM32H7RS officially support all data sizes from 4 to 16 bits?
- If so, could IS_SPI_LIMITED_DATASIZE be updated to accept SPI_DATASIZE_4BIT to SPI_DATASIZE_16BIT in a future release?
- Could the Table 578 header and FIFO threshold row be reviewed?

Thank you.

Best answer by Saket_Om

Hello ​@macosali 

Thank you for bringing this issue to our attention.

I reported this internally.

Internal ticket number: CDM0066202 (This is an internal tracking number and is not accessible or usable by customers).

3 replies

macosaliAuthor
Associate
September 24, 2026

Update: I found a second limited-instance check with the same root cause, this time on SPI4, which drives an external SPI flash.

 

In stm32h7rsxx_hal_spi.h, the transfer size for limited instances is capped at 1022:

 

  #define IS_SPI_LIMITED_TRANSFER_SIZE(SIZE) (((SIZE) < 0x3FFU) && ((SIZE) != 0U))

  #define IS_SPI_TRANSFER_SIZE(SIZE) (((SIZE) < 0xFFFFU) && ((SIZE) != 0U))

 

IS_SPI_LIMITED_TRANSFER_SIZE is asserted in all nine transfer functions (HAL_SPI_Transmit, HAL_SPI_Receive and HAL_SPI_TransmitReceive, in their blocking, IT and DMA variants). However, RM0477 Table 578 (the same table as in my first post) states "Number of data control (TSIZE): up to 65535" for SPI4 and SPI5.

 

Test on hardware: with the assert bypassed, a 4096-byte transfer on SPI4 completes correctly with EOT, and the data read back from the flash matches what was written. This is a meaningful check, because 4096 = 0x1000 has all lower 10 bits cleared. If TSIZE were only 10 bits wide on SPI4, the hardware would see TSIZE = 0 (endless transfer) and EOT would never be set.

 

The pattern is the same as for IS_SPI_LIMITED_DATASIZE: the STM32U5 and STM32H5 HAL use the same < 0x3FF limit, while the STM32N6 HAL uses < 0xFFFF for limited instances as well.

 

Minor side note: both macros use a strict < comparison, so the boundary values themselves (1023 and 65535) are also rejected, although TSIZE can hold them.

 

Additional question:

- Can ST confirm that TSIZE on SPI4/SPI5 of STM32H7RS is a full 16-bit field, and could IS_SPI_LIMITED_TRANSFER_SIZE be aligned with RM0477 in a future release?

 

Thank you.

Saket_OmBest answer
ST Technical Moderator
October 2, 2026

Hello ​@macosali 

Thank you for bringing this issue to our attention.

I reported this internally.

Internal ticket number: CDM0066202 (This is an internal tracking number and is not accessible or usable by customers).

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om
macosaliAuthor
Associate
October 2, 2026

Hello.

Thanks lot.

Could you also check this  DSB Solve

This is also from our team.