Skip to main content
BRobe.3
Associate III
Oct 17, 2024 9:12 AM UTC
Solved

stm32h7disco-i2s-baremetal(in stm32h7-i2s-record-play-wav-master)

I try for the first time to use audio , on my stm32h747i-DISCO board.

I have 2 questions

1) the build CM7 is showing the following error

Description Resource Path Location Type

'Mode' undeclared (first use in this function) stm32h7xx_hal_msp.c /stm32h7disco-i2s-baremetal_CM7/Core/Src line 179 C/C++ Problem

in

/* USER CODE END I2S1_Init 1 */

hi2s1.State = HAL_I2S_STATE_RESET;

hi2s1.Instance = SPI1;

hi2s1.Init.Mode = Mode;

hi2s1.Init.Standard = I2S_STANDARD_PHILIPS;

hi2s1.Init.DataFormat = I2S_DATAFORMAT_16B_EXTENDED;

hi2s1.Init.MCLKOutput = I2S_MCLKOUTPUT_DISABLE;

hi2s1.Init.AudioFreq = I2S_AUDIOFREQ_11K;

hi2s1.Init.CPOL = I2S_CPOL_LOW;

hi2s1.Init.FirstBit = I2S_FIRSTBIT_MSB;

hi2s1.Init.WSInversion = I2S_WS_INVERSION_DISABLE;

hi2s1.Init.Data24BitAlignment = I2S_DATA_24BIT_ALIGNMENT_RIGHT;

hi2s1.Init.MasterKeepIOState = I2S_MASTER_KEEP_IO_STATE_DISABLE;

if (HAL_I2S_Init(&hi2s1, Mode) != HAL_OK) //This Mode is the error

{

Error_Handler();

}

/* USER CODE BEGIN I2S1_Init 2 */

/* USER CODE END I2S1_Init 2 */

}

Even after regenerating the code, the error is still here

 

  1. I imagine the input is Jack microphone aud the output is Jack speaker.

The notice says I2S pins

- PA4: i2s1_ws

- PA6: i2s1_sdi :Digital pin5 of the arduino connector below the Disco Module.

- PB3: i2s1_ck

- PD7: i2s1_sdo I am not usual of I2S, may be the output is I2S1_SDO pin (But, I don't see any access to this pin).



This topic has been closed for replies.
Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
Oct 17, 2024 9:33 AM UTC

You are probably referring to Github project of gokmez?

Have you already contacted him and asked him about it?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

6 replies

Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
Oct 17, 2024 9:33 AM UTC

You are probably referring to Github project of gokmez?

Have you already contacted him and asked him about it?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
BRobe.3
BRobe.3Author
Associate III
Oct 17, 2024 12:33 PM UTC

Thanks for your answer. Yes it is https://github.com/gokmez/stm32h7-i2s-record-play-wav.

I will try contact him

Best regards

mƎALLEm
ST Technical Moderator
Oct 17, 2024 9:39 AM UTC

Hello @BRobe.3 ,


@BRobe.3 wrote:

I try for the first time to use audio , on my stm32h747i-DISCO board.


Which Demo? you need always to provide details from the beginning to prevent confusions ..

Also, please use </> button to share your code. Refer to the tips on how to post a thread.

Thank you.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
BRobe.3
BRobe.3Author
Associate III
Oct 17, 2024 12:36 PM UTC

Thanks for your answer

It is : https://github.com/gokmez/stm32h7-i2s-record-play-wav for   stm32h747i-DISCO board.

Best Regards