stm32h7b3i-dk SAI1 configuration
- 4 replies
- 922 views
Hi,
I am trying to use SAI instead of I2S6 since the BDMA seems to not trigger even after proper configuration.
I am using SAI for the first time so I am completely unsure about this config:
/**
* @brief SAI1 Initialization Function
* @PAram None
* @retval None
*/
static void MX_SAI1_Init(void)
{
/* USER CODE BEGIN SAI1_Init 0 */
/* USER CODE END SAI1_Init 0 */
/* USER CODE BEGIN SAI1_Init 1 */
/* USER CODE END SAI1_Init 1 */
hsai_BlockA1.Instance = SAI1_Block_A;
hsai_BlockA1.Init.AudioMode = SAI_MODEMASTER_TX;
hsai_BlockA1.Init.Synchro = SAI_ASYNCHRONOUS;
hsai_BlockA1.Init.OutputDrive = SAI_OUTPUTDRIVE_DISABLE;
hsai_BlockA1.Init.NoDivider = SAI_MASTERDIVIDER_ENABLE;
hsai_BlockA1.Init.FIFOThreshold = SAI_FIFOTHRESHOLD_1QF;
hsai_BlockA1.Init.AudioFrequency = SAI_AUDIO_FREQUENCY_22K;
hsai_BlockA1.Init.SynchroExt = SAI_SYNCEXT_DISABLE;
hsai_BlockA1.Init.MonoStereoMode = SAI_STEREOMODE;
hsai_BlockA1.Init.CompandingMode = SAI_NOCOMPANDING;
hsai_BlockA1.Init.TriState = SAI_OUTPUT_NOTRELEASED;
if (HAL_SAI_InitProtocol(&hsai_BlockA1, SAI_I2S_STANDARD, SAI_PROTOCOL_DATASIZE_16BIT, 2) != HAL_OK)
{
Error_Handler();
}
hsai_BlockB1.Instance = SAI1_Block_B;
hsai_BlockB1.Init.AudioMode = SAI_MODESLAVE_RX;
hsai_BlockB1.Init.Synchro = SAI_SYNCHRONOUS;
hsai_BlockB1.Init.OutputDrive = SAI_OUTPUTDRIVE_DISABLE;
hsai_BlockB1.Init.FIFOThreshold = SAI_FIFOTHRESHOLD_1QF;
hsai_BlockB1.Init.SynchroExt = SAI_SYNCEXT_DISABLE;
hsai_BlockB1.Init.MonoStereoMode = SAI_STEREOMODE;
hsai_BlockB1.Init.CompandingMode = SAI_NOCOMPANDING;
hsai_BlockB1.Init.TriState = SAI_OUTPUT_NOTRELEASED;
if (HAL_SAI_InitProtocol(&hsai_BlockB1, SAI_I2S_STANDARD, SAI_PROTOCOL_DATASIZE_16BIT, 2) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN SAI1_Init 2 */
/* USER CODE END SAI1_Init 2 */
}DMA seems to be working and I am getting a values of around 65000 , so I suspect the audio driver or SAI configuration is wrong.
I have taken some portion of the audio driver from the stm32 repo . I was unsure how to use the driver also It gave me some errors when I included it in my build (some functions had same name as the CubeMx generated ones).
I2C in the driver works and I confirmed this by reading the ID from the Codec. I can read and write registers . So I have created few functions to setup MIC and start it.
SAI configuration is shown above , and DMA was also configured using the GUI . which seems to work and read some values but these values are either close to zero or close to 65000 all the time.