Skip to main content
Marius CO
Associate II
Feb 4, 2023 12:24 AM UTC
Question

STM32H7A3 STM32H7A3ZIT6Q CDC_Transmit_HS Speed limit about to 600.000 Octets/second

I have an ADC+DMA read that can performs at 4Mbytes/second.

The conv is 12 bit, clock division is 1_of5. On the callback DMS interrupts

I send half data's to USB using CDC_Transmit_HS.

The ADC buffer is 1K. I Also tried 2, 4, 8, 16k. I played with the clock division for ADC and

conversion cycles to tweak the ADC speed up to the point the . CDC_Transmit_HS returns USB_BUSY. The maximum rate I could achieve was 592896 bytes /second, (no send errors) I guess with division 1 and 3conv_5 cycles. The host was Linux and Windows (same cutt of speed)

My target is 1M bytes/second as the USB can go up to 40Mbits /second -> 3Mbytes/second.

Where I am wrong here ?

void HAL_PCD_MspInit(PCD_HandleTypeDef* pcdHandle)
{
 GPIO_InitTypeDef GPIO_InitStruct = {0};
 RCC_PeriphCLKInitTypeDef PeriphClkInitStruct = {0};
 if(pcdHandle->Instance==USB_OTG_HS)
 {
 /* USER CODE BEGIN USB_OTG_HS_MspInit 0 */
 
 /* USER CODE END USB_OTG_HS_MspInit 0 */
 
 /** Initializes the peripherals clock
 */
 PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_USB;
 PeriphClkInitStruct.UsbClockSelection = RCC_USBCLKSOURCE_HSI48;
 if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)
 {
 Error_Handler();
 }
 
 /** Enable USB Voltage detector
 */
 HAL_PWREx_EnableUSBVoltageDetector();
 
 __HAL_RCC_GPIOA_CLK_ENABLE();
 /**USB_OTG_HS GPIO Configuration
 PA8 ------> USB_OTG_HS_SOF
 PA9 ------> USB_OTG_HS_VBUS
 PA10 ------> USB_OTG_HS_ID
 PA11 ------> USB_OTG_HS_DM
 PA12 ------> USB_OTG_HS_DP
 */
 GPIO_InitStruct.Pin = GPIO_PIN_8|USB_FS_ID_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH; // GPIO_SPEED_FREQ_LOW; // mco-
 GPIO_InitStruct.Alternate = GPIO_AF10_OTG1_HS;
 HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
 
 GPIO_InitStruct.Pin = USB_FS_VBUS_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 HAL_GPIO_Init(USB_FS_VBUS_GPIO_Port, &GPIO_InitStruct);
 
 GPIO_InitStruct.Pin = USB_FS_N_Pin|USB_FS_P_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;// GPIO_SPEED_FREQ_LOW; // mco-
 HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
 
 /* Peripheral clock enable */
 __HAL_RCC_USB_OTG_HS_CLK_ENABLE();
 
 /* Peripheral interrupt init */
 HAL_NVIC_SetPriority(OTG_HS_IRQn, 0, 0);
 HAL_NVIC_EnableIRQ(OTG_HS_IRQn);
 /* USER CODE BEGIN USB_OTG_HS_MspInit 1 */
 
 /* USER CODE END USB_OTG_HS_MspInit 1 */
 }
}

Thank you.

This topic has been closed for replies.

1 reply

AScha.3
Super User
Feb 4, 2023 12:23 PM UTC

> Where I am wrong here ?

  1. USB full speed has 12 Mbit .
  2. max. data load depends on overhead and use by other members
  3. i got about 1 MB/s (with CDC) , what is close to maximum in real world, i suppose.

so your 0,6MB is quite good.

If you feel a post has answered your question, please click on " Best Answer ".