Skip to main content
Associate II
Nov 24, 2025 11:36 AM UTC
Question

STM32H755 – End-of-Frame Detection Fails Only with EventFlags, Works with Polling

Hello ST Team,

I am using an STM32H755ZIT6 where CM7 handles a high-speed Quad-SPI flash interface with 100Mhz and UART communication with flow control 115200 baud.
The same firmware runs on two hardware revisions:

  • Revision V2: Works perfectly

  • Revision V3: Same firmware → occasional failure in UART frame processing

The QSPI itself receives data correctly (verified with CRC), but the “end of frame” indication is occasionally not processed.


Observed Firmware Behavior

1. Using RTOS Event Flags (original implementation)

In the UART receive callback, when “end of frame” (EOF) is detected, we set an RTOS event flag:

 

 
osEventFlagsSet(dataReceiveEvent, DataReceived);

Problem on V3:

  • Sometimes the event flag is not triggered

  • Even though all received bytes are correct

  • CRC validation passes

  • The callback executes, but the main task does not wake

This leads to missed packets even though the data is fully received.


2. Switching to Polling Loop (temporary workaround)

We replaced the RTOS event flag with a simple polling mechanism inside the processing task:

 
 
while(1) 
{ 
 if(osMessageQueueGet(...) == osOK)
 process(); 
 osDelay(10); 
}

With this change:

  • V3 hardware works consistently

  • No EOF detection failures

  • No lost frames

  • V2 continues to work as usual

This confirms the raw UART data is always correct — only the timing window of the RTOS wake-up is sensitive.


3. Interpretation (What I need ST guidance on)

It appears that:

  • The UART ISR + RTOS event-flag + context switching timing is borderline in some conditions

  • Minor timing jitter causes occasional missed RTOS event wakeups

  • Polling hides this issue because it does not depend on a precise timing window


4. Questions for ST

  1. Are there known conditions where CMSIS-RTOS2 EventFlags used inside UART RX callbacks can be missed due to timing jitter or interrupt priority interactions?

  2. Is there any recommendation on:

    • Minimum ISR execution time

    • Maximum recommended operations inside UART RX callback

    • Priority level requirements for tasks waiting on EventFlags

  3. Does ST recommend using:

    • Ring buffer + task polling

    • Direct-to-queue from ISR

    • Stream buffer

    • Event flags
      for continuous, critical UART communication?

  4. Any known errata for STM32H7 regarding:

    • EventFlags not waking tasks

    • Interrupt latency

    • Missed wakeups under high-load conditions


5. Summary

  • Data reception is always correct

  • CRC is valid

  • Only the RTOS event flag wake-up occasionally fails

  • Polling solves the problem

  • Need guidance on recommended ISR → task signaling method for STM32H7

Thank you in advance.

4 replies

ST Technical Moderator
Nov 24, 2025 2:45 PM UTC

Hello @Ibrahimsha 

To ensure reliable signaling between the UART interrupt and your RTOS task (for example, when using EventFlags or other RTOS primitives), it is essential to configure the UART interrupt priority correctly. For example, if your RTOS kernel allows API calls from ISRs with priority values of 5 or higher, set the UART interrupt priority to 5, 6, or a higher number.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om
Associate II
Nov 24, 2025 4:34 PM UTC

Hello @Saket_Om,

Thank you for the clarification.

I have verified the NVIC configuration, and all UART interrupts that interact with FreeRTOS are already configured at priority level 5, which is within the valid range for FreeRTOS ISR APIs (numerically ≥ configLIBRARY_MAX_SYSCALL_INTERRUPT_PRIORITY).

✔ UART1 global interrupt → Priority 5
✔ UART7 global interrupt → Priority 5
✔ QUADSPI, DMA, and I2C interrupts that call RTOS functions are also configured at priority 5

So the interrupt priorities are already set correctly according to the FreeRTOS requirements and should not cause ISR-to-task signaling issues.

I think this is correct. If anything looks wrong, kindly guide me.

Thank you for your support.

ST Technical Moderator
Nov 25, 2025 1:49 PM UTC

Hello @Ibrahimsha 

Did you try with peripheral interrupt priorities > 5 ?

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om
Associate II
Nov 26, 2025 6:04 AM UTC


Hello @Saket_Om,

Yes, I tested using peripheral interrupt priorities greater than 5 (including priority 6) as recommended.

To provide complete visibility, here is the runtime NVIC priority table captured from the STM32H755:

 


================ NVIC PRIORITY DEBUG ================
Priority Grouping = 3 (0=NVIC_PRIORITYGROUP_0 ... 4=NVIC_PRIORITYGROUP_4)

IRQ Priority Pending
--------------------------
7 5 0 <-- UART-related
11 5 0
28 4 0
52 5 0
53 5 0
82 5 0
101 5 0

 


All UART, QSPI, DMA, and I2C interrupts that interact with RTOS APIs are assigned:

Priority 5 or 6

Priority grouping value that respects
configLIBRARY_MAX_SYSCALL_INTERRUPT_PRIORITY = 5

We also changed some peripheral priorities from 5 to 6 (e.g., QUADSPI, UART) specifically for this investigation.

So the ISR priority configuration is correct and should not cause missed RTOS wakeups.

✔ Old Implementation (Works on V2, fails intermittently on V3)
This version uses EventFlags for ISR → Task signaling:

 


memset(&processData, 0, sizeof(ProcessData)); dataSize = inDataBufferIndex; processData.size = inDataBufferIndex; memset(&processData.receivedDataBuffer, 0, sizeof(receivedBuffer)); memcpy(&processData.receivedDataBuffer, receivedBuffer, dataSize); if (osMessageQueueGetSpace(ISCMessageQueue) > 0) { if (osMessageQueuePut(ISCMessageQueue, &processData, MessagePriority, QueueAccessTimeOutInMS) == osOK) { osEventFlagsSet(dataReceiveEvent, DataReceived); } } else { DebugLog("data error - Queue Full\r\n"); osEventFlagsSet(dataReceiveEvent, DataReceived); }

 

Behavior:
On V2 hardware → works perfectly

On V3 hardware → data is received correctly, CRC is valid, ISR executes, and the queue is updated
but the task occasionally does not wake from osEventFlagsWait()

In this case, osEventFlagsWait() returns osErrorResource (-3), even though the ISR was executed and data was placed in the queue.

This results in missing “end-of-frame” notifications even though the data path is correct.

✔ New Implementation (Stable on V3)
Changing the signaling from EventFlags to ThreadFlags made the system fully reliable on V3:

 


memset(&processData, 0, sizeof(ProcessData)); dataSize = inDataBufferIndex; processData.size = inDataBufferIndex; memset(&processData.receivedDataBuffer, 0, sizeof(receivedBuffer)); memcpy(&processData.receivedDataBuffer, receivedBuffer, dataSize); if (osMessageQueueGetSpace(ISCMessageQueue) > 0) { if (osMessageQueuePut(ISCMessageQueue, &processData, MessagePriority, QueueAccessTimeOutInMS) == osOK) { osThreadFlagsSet(dataReceivingTaskHandle, DataReceived); } } else { DebugLog("data error - Queue Full\r\n"); osThreadFlagsSet(dataReceivingTaskHandle, DataReceived); }

Result:
V3 hardware becomes fully stable

No missed wake-ups

No frame-processing failures

V2 continues to work exactly as before

✔ What I Am Trying to Understand
From my observations:

EventFlags seem more sensitive to ISR timing and may lose the wake-up if the event is set before the task enters osEventFlagsWait().

ThreadFlags appear strictly 1:1 and consistently wake the correct task without missing notifications.

:question_mark: Questions
Are there known differences in wake-up semantics between EventFlags and ThreadFlags when used from a UART ISR on STM32H7?

Is EventFlags more prone to race conditions in ISR → Task signaling compared to ThreadFlags?

Does ST recommend ThreadFlags, or direct-to-queue notification, instead of EventFlags for high-frequency UART communication?

Is there any STM32H7 or CMSIS-RTOS2 errata related to missed EventFlags wakeups or ISR → Task synchronization?

The data reception itself is correct in all cases—only the RTOS wake-up mechanism differs in reliability between EventFlags and ThreadFlags.

FYI

================ NVIC PRIORITY DEBUG ================
Priority Grouping = 3 (0=NVIC_PRIORITYGROUP_0 ... 4=NVIC_PRIORITYGROUP_4)

Active IRQ = -16

IRQ   Priority   Pending
--------------------------
  0       0        0
  1       0        0
  2       0        0
  3       0        0
  4       0        0
  5       0        0
  6       0        0
  7       5        0
  8       0        0
  9       0        0
 10       0        0
 11       5        0
 12       0        0
 13       0        0
 14       0        0
 15       0        0
 16       0        0
 17       0        0
 18       0        0
 19       0        0
 20       0        0
 21       0        0
 22       0        0
 23       0        0
 24       0        0
 25       0        0
 26       0        0
 27       0        0
 28       4        0
 29       0        0
 30       0        0
 31       0        0
 32       0        0
 33       0        0
 34       0        0
 35       0        0
 36       0        0
 37       0        0
 38       0        0
 39       0        0
 40       0        0
 41       0        0
 42       0        0
 43       0        0
 44       0        0
 45       0        0
 46       0        0
 47       0        0
 48       0        0
 49       0        0
 50       0        0
 51       0        0
 52       5        0
 53       5        0
 54       0        0
 55       0        0
 56       0        0
 57       0        0
 58       0        0
 59       0        0
 60       0        0
 61       0        0
 62       0        0
 63       0        0
 64       0        0
 65       0        1
 66       0        0
 67       0        0
 68       0        0
 69       0        0
 70       0        0
 71       0        0
 72       0        0
 73       0        0
 74       0        0
 75       0        0
 76       0        0
 77       0        0
 78       0        0
 79       0        0
 80       0        0
 81       0        0
 82       5        0
 83       0        0
 84       0        0
 85       0        0
 86       0        0
 87       0        0
 88       0        0
 89       0        0
 90       0        0
 91       0        0
 92       0        0
 93       0        0
 94       0        0
 95       0        0
 96       0        0
 97       0        0
 98       0        0
 99       0        0
100       0        0
101       5        0
102       0        0
103       0        0
104       0        0
105       0        0
106       0        0
107       0        0
108       0        0
109       0        0
110       0        0
111       0        0
112       0        0
113       0        0
114       0        0
115       0        0
116       0        0
117       0        0
118       0        0
119       0        0
120       0        0
121       0        0
122       0        0
123       0        0
124       0        0
125       0        0
126       0        0
127       0        0
128       0        0
129       0        0
130       0        0
131       0        0
132       0        0
133       0        0
134       0        0
135       0        0
136       0        0
137       0        0
138       0        0
139       0        0
140       0        0
141       0        0
142       0        0
143       0        0
144       0        0
145       0        0
146       0        0
147       0        0
148       0        0
149       0        0
150       0        0
151       0        0
152       0        0
153       0        0
154       0        0
155       0        0
156       0        0
157       0        0
158       0        0
159       0        0
160       0        0
161       0        0
162       0        0
163       0        0
164       0        0
165       0        0
166       0        0
167       0        0
168       0        0
169       0        0
170       0        0
171       0        0
172       0        0
173       0        0
174       0        0
175       0        0
176       0        0
177       0        0
178       0        0
179       0        0
180       0        0
181       0        0
182       0        0
183       0        0
184       0        0
185       0        0
186       0        0
187       0        0
188       0        0
189       0        0
190       0        0
191       0        0
192       0        0
193       0        0
194       0        0
195       0        0
196       0        0
197       0        0
198       0        0
199       0        0
200       0        0
201       0        0
202       0        0
203       0        0
204       0        0
205       0        0
206       0        0
207       0        0
208       0        0
209       0        0
210       0        0
211       0        0
212       0        0
213       0        0
214       0        0
215       0        0
216       0        0
217       0        0
218       0        0
219       0        0
220       0        0
221       0        0
222       0        0
223       0        0
224       0        0
225       0        0
226       0        0
227       0        0
228       0        0
229       0        0
230       0        0
231       0        0
232       0        0
233       0        0
234       0        0
235       0        0
236       0        0
237       0        0
238       0        0
239       0        0

 


Thank you again for your guidance.
I appreciate your continued support.