Skip to main content
Associate II
Nov 4, 2025 2:48 PM UTC
Solved

stm32h755 Clock setup: HAL_RCC_ClockConfig returns error.

Hi all,

I am having issues with Clock setup for Stm32h755. Especially regarding the M4 core. Currently, I only run the M4 core. The M7 core has no valid firmware. Is that even a supported mode?

I try to setup a rather basic clock setup but the setup keeps failing at the call: HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_4), which will return an not ok return value.

I also tried using HSI and other different setups. But it seems the keep failing in the same way. Interestingly... When I simply ignore the error. Then most stuff seems to work just fine. I got ADC, SPI, Timers working. However, I am not sure where the issue is with the clock configuration.

The entire clock setup: 

static void SystemClock_Config(void) {
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

 __HAL_RCC_SYSCFG_CLK_ENABLE();

 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI | RCC_OSCILLATORTYPE_HSE;
 RCC_OscInitStruct.HSEState = RCC_HSE_ON;
 RCC_OscInitStruct.HSIState = RCC_HSI_ON;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
 RCC_OscInitStruct.PLL.PLLM = 5;
 RCC_OscInitStruct.PLL.PLLN = 192;
 RCC_OscInitStruct.PLL.PLLP = 2;
 RCC_OscInitStruct.PLL.PLLQ = 2;
 RCC_OscInitStruct.PLL.PLLR = 2;
 RCC_OscInitStruct.PLL.PLLRGE = RCC_PLL1VCIRANGE_2;
 RCC_OscInitStruct.PLL.PLLVCOSEL = RCC_PLL1VCOWIDE;
 RCC_OscInitStruct.PLL.PLLFRACN = 0;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK) {
 // print error
 }

 /** Initializes the CPU, AHB and APB buses clocks
 */
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK | RCC_CLOCKTYPE_SYSCLK | RCC_CLOCKTYPE_PCLK1 |
 RCC_CLOCKTYPE_PCLK2 | RCC_CLOCKTYPE_D3PCLK1 | RCC_CLOCKTYPE_D1PCLK1;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
 RCC_ClkInitStruct.SYSCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_HCLK_DIV2;
 RCC_ClkInitStruct.APB3CLKDivider = RCC_APB3_DIV2;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_APB1_DIV2;
 RCC_ClkInitStruct.APB2CLKDivider = RCC_APB2_DIV2;
 RCC_ClkInitStruct.APB4CLKDivider = RCC_APB4_DIV2;

 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_4) != HAL_OK) {
 // print error
 }
}


Best regards

Mark


Edited to apply proper source code formatting - please see How to insert source code for future reference.

Mark12Best answer
Associate II
Nov 5, 2025 8:58 AM UTC

Hi,

this was a good lead that showed me the real problem. There was a missing call to Hal_Init(). Which caused the tickPriority to not be set.

 

Thanks & Best regards

Mark

7 replies

TDK
Nov 4, 2025 3:06 PM UTC

The clock failing to start can suggest the HSE design is not correct. Perhaps incorrect load caps.

Guidelines for oscillator design on STM8AF/AL/S and STM32 MCUs/MPUs - Application note

 

M4 having no firmware is fine. You can set option bytes such that the M4 core doesn't boot, but it's not an issue here.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Andrew Neil
Super User
Nov 4, 2025 3:43 PM UTC

@Mark12 wrote:

the call: HAL_RCC_ClockConfig( &RCC_ClkInitStruct, FLASH_LATENCY_4 ), which will return an not ok return value..


Have you tried stepping into that function to see where & why, exactly, it is failing?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Mark12Author
Associate II
Nov 4, 2025 8:58 PM UTC

Hi Andrew,

I stepped inside and it seems to fail in:

__weak HAL_StatusTypeDef HAL_InitTick(uint32_t TickPriority)

 

more precisely in this check:

/* Configure the SysTick IRQ priority */
if (TickPriority < (1UL << __NVIC_PRIO_BITS))
{
 HAL_NVIC_SetPriority(SysTick_IRQn, TickPriority, 0U);
 uwTickPrio = TickPriority;
}
else
{
 // will return ERROR here
 return HAL_ERROR;
}
 

Edited to apply proper source code formatting - please see How to insert source code for future reference.

mƎALLEm
ST Technical Moderator
Nov 4, 2025 4:50 PM UTC

Hello,

Which board are you using? Nucleo board?

If it's the case, you need to set HSE in Bypass mode as the clock source is provided from the STLINK (STLINK_MCO) and there is no crystal on the board:

mALLEm_0-1762275019446.png

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Mark12Author
Associate II
Nov 4, 2025 9:11 PM UTC

Hi,

yes. I am on a nucleo board. I tried setting HSE_Bypass but it didnt change the behavior. The Config method fails on the method 

HAL_InitTick

Because of what seems to be an invalid TickPriority of "16" which is somehow present. 

 

Edited to apply proper source code formatting - please see How to insert source code for future reference.

TDK
Nov 4, 2025 9:41 PM UTC

16 is not a valid priority. Change it to 15 or less.

TDK_0-1762292476257.png

 

Include your IOC file if you're having trouble.

"If you feel a post has answered your question, please click ""Accept as Solution""."