Associate II
January 29, 2026
Solved
STM32H753ZI Ethernet (LAN8742, RMII) – Ping not working with HAL / No-RTOS lwIP
- 6 replies
- 697 views
I am using STM32H753ZI and trying to bring up Ethernet (LAN8742, RMII) using HAL + lwIP in NO-RTOS mode. I generated the code using STM32CubeMX with ETH enabled (RMII) and lwIP enabled (WITH_RTOS disabled, static IP). The PHY link comes up and RJ45 LEDs blink, but the board does not respond to ping and no ARP entry is created on the PC (Destination Host Unreachable). I have placed ETH descriptors and RX buffers in D2 SRAM, enabled MPU and D-Cache, verified RMII_REF_CLK to PA1, selected the LAN8742 PHY driver, and I am calling MX_ETH_Init(), MX_LWIP_Init(), and processing lwIP in the main loop. The FreeRTOS-based STM32H743 Ethernet example works, but I specifically want a HAL-only .