Skip to main content
Ocebe.1
Associate II
Feb 26, 2025 4:44 PM UTC
Question

STM32H753 PING STOPPED

Hello, I am working on Ethernet with the STM32H753 board. After configuring the necessary Ethernet settings, I can ping the assigned IP address of the board. However, after a few minutes, I can no longer ping it. What could be the reason for this issue?

I am using STM32CubeIDE version 1.17.0 and library version 1.12.0.

Thank you for your help!

This topic has been closed for replies.

3 replies

mbarg.1
Senior III
Feb 26, 2025 5:15 PM UTC

You must share the project or we can just bet on some possible cause - like: you are not releasing packets and you run out of resources - but could be onything else

Andrew Neil
Super User
Feb 26, 2025 5:32 PM UTC

So what debugging have you done to find what's happening?

Put some diagnostics into your code so that you can see what's going on.

As @mbarg.1 said, you've given nothing to go on - but anything which stops working "after a while" smells of resources being used but not released when done ...

 

How to write your question to maximize your chances to find a solution

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
ST Employee
Feb 27, 2025 2:01 PM UTC

Hello @Ocebe.1,

This post might help you: Solved: unable to ping ethernet connection with stm32h7 - STMicroelectronics Community

You can find a ping example there that can assist you in correctly pinging your board.

 

With Regards,

"If your question is answered, please close this topic by clicking ""Accept as Solution""."