Skip to main content
YHail.1
Visitor II
Jan 25, 2023 9:01 AM UTC
Question

STM32H750XB USB I/Fs

Hi

On STM32H750XB datasheet it says 2 x USBUSB OTG interfaces (1FS, 1HS/FS) .

I configured the 1st port as FS, and the 2nd port as HS which connectd to external PHY (internal FS phy disabled) .

I want to confirm that if the 2 ports can be used at different speed (1 as FS and 1 as HS) at the same time just for sure.

Thanks

This topic has been closed for replies.

1 reply

ST Technical Moderator
Jan 25, 2023 12:20 PM UTC

Hello @YHail.1​ and welcome to the Community :)

I confirm that both instances should work at the same time.

When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks