Question
STM32H750VBT External Loader for W25Q64JVSSIQ
- 3 replies
- 93 views
Erase sector operation is failing for more than 2 sectors
I have attached the code base
ignore trace functionality added for debugging
0x20 function code, (Not clear if the call to erase sector are separate or single call)
write enable, erase command, wait for Busy bit to be cleared
Can someone help to spot the issue