Skip to main content
Associate
Oct 17, 2023 9:36 AM UTC
Solved

STM32H745xi enter standby mode after power on 3 seconds

I use STM32H745xi discovery board. When i do some test, i download code that Cortex-m7 will enter standby mode after power on 3 seconds. And i set wrong wakeup pin(wakeup pin 1&not config PA0, it should be wakeu4). After power off and power on, i find that it can't recognize the mcu through ST-LINK though i try RST pin. I dont understand why RST pin not work.

Pls help to save the board,thx.

 

 

code:

 MX_GPIO_Init();
HAL_Delay(3000);
HAL_PWR_EnableWakeUpPin(PWR_WAKEUP_PIN1);
while (1)
{
HAL_PWR_EnterSTANDBYMode();
HAL_GPIO_TogglePin(GPIOJ,4);
HAL_Delay(500);
}

This topic has been closed for replies.
Jerry3Best answer
Associate
Oct 18, 2023 8:03 AM UTC

I change boot0 from 0 to 1. And download correct code. Then change boot0 from 0 to 1, the problem is solved

3 replies

ST Employee
Oct 17, 2023 10:24 AM UTC

Welcome @Jerry3  to ST Community, 

Try connecting "under reset" with STM32CubeProgrammer 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Jerry3Author
Associate
Oct 18, 2023 1:43 AM UTC

Hi Sarrs,

    It seems not work. I press RST pin and connect with STM32CubeProgrammer  through ST-LINK

Jerry3AuthorBest answer
Associate
Oct 18, 2023 8:03 AM UTC

I change boot0 from 0 to 1. And download correct code. Then change boot0 from 0 to 1, the problem is solved