Skip to main content
Associate
July 19, 2024
Question

STM32H745 DAMMUX1 not configurable if any one of the DMA block reset

Hi,

I am using the STM32H745 and facing the following issue:

  1. ADC with DMA1 works fine when the DMA2 block is not reset.
  2. ADC with DMA1 fails when the DMA2 block is reset(in RCC->AHB1RSTR). The "DMAMUX request line multiplexer (DMAREQ_ID field in the DMAMUX_C0CR register)" resets back to 0.

It appears that the DMAMUX is closely tied to both DMA controllers (DMA1 and DMA2). None of the available documents (es0445-stm32h745-errata, rm0399 - Reference Manual, en.STM32H7-DMAMUX, en.STM32H7-DMA) provide the required information on this behavior.

Is this the expected behavior? Are there any documents from STM32 that can justify this? some help would be greatly appreciated. 

Thanks

 

This topic has been closed for replies.

4 replies

nouirakh
ST Employee
August 21, 2024

Hello @shivashankarr 

In order to reproduce the possible issue, could you please provide more details on your setting project if possible, attach your .ioc file/configuration?

Associate
August 21, 2024

Hello nouirakh,

Sorry, this is a non-IOC file setup, but I can provide detailed steps to reproduce the issue.

Case 1: Configure the ADC and DMA1 to interface with any sensor or memory, then reset DMA2 (in RCC->AHB1RSTR). Afterward, check the SFR register the DMAREQ_ID field in the DMAMUX_C0CR register will reset to 0.

Case 2: If you reset DMA2 (in RCC->AHB1RSTR) and then try to configure the ADC and DMA1, observe the SFR register (DMAREQ_ID field in the DMAMUX_C0CR register). It will not allow you to write the configuration.

BR

ST Technical Moderator
August 30, 2024

Hello @shivashankarr 

 

I escalated this post internally and will be back to you with update.

Internal Ticket ID 189893 (It is an internal tracking number and is not accessible or usable by customers).

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om
ST Technical Moderator
November 12, 2024

Hello @shivashankarr 

After investigation, we confirm that this is the expected behavior. The reference manual will be updated to include this information for clarity.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om