Skip to main content
Visitor II
Dec 6, 2024 9:15 AM UTC
Question

STM32H743iiK6 project with SD card not working

Hi,

   I worked for last three weeks STM32H743iik6 project with SD card .SD card with SPI interface but I got FR_NOT_READY error.I have checked hardware connection.same code work in stm32f and stm32 l series.I don't know reason for stm32h series not working.please any one have code stm32h series please send me.

 

 

 

This topic has been closed for replies.

2 replies

Danish1
Lead III
Dec 6, 2024 10:01 AM UTC

Stm32h7xx is very different from stm32f4 and stm32l, in that it uses many more caches and other performance-enhancing techniques. Unless you add things like __dsb() and cache-related code where necessary (I explicitly disable cacheing in memory-regions where I use DMA, but ST seem to favour explicit flushing/invalidating before/after DMA) you are likely to hit problems.

This is a bit of a long-shot. What revision is your stm32h743?

Years ago I started a project around a stm32h743 (actually trying to port from a board that took stm32f767 because I wanted more RAM). But I have up after struggling for a long time with the SD-card interface. This was with stm32h743 Revision Y, which has loads of errata to do with its sdmmc peripheral.

I have recently revisited the project using the newer Revision V that has many of the sdmmc errata fixed. The sdmmc bit currently works (based on HAL; I am not a fan of HAL and I intend to rewrite the code when I get the opportunity).

ST Technical Moderator
Dec 6, 2024 10:38 AM UTC

Hello @SK52  

Please refer to the example Projects/STM32H743I-EVAL/Examples/SD in the STM32CubeH7 firmware as a starting point for your application.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om