Skip to main content
LFjær.1
Associate
Mar 23, 2022 12:19 PM UTC
Question

STM32H743 with USB HS, FUSB2805 not detected

I have a custom board with STM32H743VIT6 connected to an external USB HS PHY, the FUSB2805MLX.

I am trying to run a bare minimum example setup in STM32CubeMx. Just including a USB HS connection and the device in USB VCP mode.

The pin setup is correct, and the external clocks on the PHY are correct (26MHz in, generates 60MHz on CLK line between MCU and PHY).

I can see that the 60Mhz line is shut down after the call to `USBD_Start(&hUsbDeviceHs)`

The data lines are pulled high at the same time.

The relevant pinout is: 

```

PA3 -> USB_OTG_HS_ULPI_DO 

PA5 -> USB_OTG_HS_ULPI_CK 

PB0 -> USB_OTG_HS_ULPI_D1 

PB1 -> USB_OTG_HS_ULPI_D2 

PB5 -> USB_OTG_HS_ULPI_D7 

PB10 -> USB_OTG_HS_ULPI_D3 

PB11 -> USB_OTG_HS_ULPI_D4 

PB12 -> USB_OTG_HS_ULPI_D5 

PB13 -> USB_OTG_HS_ULPI_D6 

PC0 -> USB_OTG_HS_ULPI_STP 

PC2_C -> USB_OTG_HS_ULPI_DIR 

PC3_C -> USB_OTG_HS_ULPI_NXT  

```

However, i cannot get this to work.

The code runs without errors and debugging through it doesn't give me any idea of what might be wrong. All functions return with HAL_OK

The computer does not detect the USB device.

`sudo dmesg | grep usb` gives the following output

```

   [27482.966148] usb usb3-port7: attempt power cycle

   [27483.622018] usb 3-7: new low-speed USB device number 32 using xhci_hcd

   [27483.622532] usb 3-7: Device not responding to setup address.

   [27483.830337] usb 3-7: Device not responding to setup address.

   [27484.041933] usb 3-7: device not accepting address 32, error -71

   [27484.173925] usb 3-7: new low-speed USB device number 33 using xhci_hcd

   [27484.174414] usb 3-7: Device not responding to setup address.

   [27484.382364] usb 3-7: Device not responding to setup address.

   [27484.589893] usb 3-7: device not accepting address 33, error -71

   [27484.590002] usb usb3-port7: unable to enumerate USB device

   [81863.025532] usb 3-3: reset full-speed USB device number 3 using xhci_hcd

   [82185.873876] usb 3-3: reset full-speed USB device number 3 using xhci_hcd

   [82306.336339] usb 3-3: reset full-speed USB device number 3 using xhci_hcd

   [82758.471075] usb 3-3: reset full-speed USB device number 3 using xhci_hcd

```

It's the same using the USB_DEVICE Middleware in Mass Storace Class mode.

Are there any tricks to getting ULPI USB HS to work on this MCU?

This topic has been closed for replies.

1 reply

Pavel A.
Mar 23, 2022 8:00 PM UTC

Does the host really see the low-speed response or nothing at all.?

Get a physical USB bus analyzer (and somebody who knows how to use it)