Skip to main content
jumman_JHINGA
Senior III
May 12, 2026
Question

STM32H743 USB Host MSC + FATFS f_opendir() Deadlock Issue in Bootloader

Hello Everyone,

I am working on a custom USB bootloader project on STM32H743 using:

  • USB Host MSC
  • FATFS
  • External QSPI Flash
  • Internal Flash update
  • IAR Workbench
  • HAL drivers

My bootloader detects USB pendrive successfully and I can see:

  • Appli_state == APPLICATION_READY
  • f_mount() returns FR_OK

But the system gets stuck / deadlocked when calling:

DIR dir;

if(f_opendir(&dir, "0:/") != FR_OK)
{
 return UPDATE_NONE;
}

The MCU hangs inside f_opendir() and never returns.

Current flow:

MX_USB_HOST_Init();

while(1)
{
 MX_USB_HOST_Process();

 if(Appli_state == APPLICATION_READY)
 {
 HAL_Delay(500);

 update_flags = ver_check();

 break;
 }
}

Inside ver_check():

if(f_mount(&USB_FatFs, USBHPath, 0) != FR_OK)
{
 return UPDATE_NONE;
}

if(f_opendir(&dir, USBHPath) != FR_OK)
{
 return UPDATE_NONE;
}

Additional Information:

  • USB Host MSC works until f_opendir()
  • No FreeRTOS used
  • USB drive detected properly
  • f_mount() succeeds
  • Deadlock occurs specifically at f_opendir()
  • Tried both "0:/" and USBHPath
  • Tried adding delays after APPLICATION_READY

    Has anyone faced f_opendir() blocking forever on H7?

Any guidance would be greatly appreciated.

Thank you.

1 reply

ST Technical Moderator
May 13, 2026

Hi @jumman_JHINGA 

Do you reproduce using firmware example? Here is an example implementing f_opendir, can you try to compare with the implementation provided?

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL