Skip to main content
Visitor II
Aug 14, 2024 3:38 PM UTC
Solved

STM32H743 USB code generation problem

I'm using an embedded hardware design based on the NUCLEO-H743ZI. Within the SMT32CubeIDE I configured all of the pins and set up the clock according to my PCB, I'm using an external LSE 32.768Khz and no external HSE. The PCB is set up to utilize VBUS sensing and ID pin, I set up the USB_OTG_FS in OTG/Dual_Role_Device with VBUS sensing. When I build and load the code on my STM I get no indication that the USB is functioning besides providing power to the PCB. What i'm expecting is to see the device accessible in REPL and it never shows up. When I change the USB_OTG_FS mode to Device_Only, which enables the Middleware USB_DEVICE option and set the class to Virtual Com Port the device has no issues making a USB connection. I noticed that in the configuration that doesn't work the code generated does not perform any function calls that include USB, only when i set it in Device_Only is when I see activity while debugging that has anything to do with USB. Is this intentional? Am I missing something?

 

    This topic has been closed for replies.
    FBLBest answer
    ST Technical Moderator
    Aug 14, 2024 5:08 PM UTC

    Hi @Erric 

    Unfortunately, Dual role device on H743 is not supported by current ST USB Middleware. 

    To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL

    1 reply

    FBLBest answer
    ST Technical Moderator
    Aug 14, 2024 5:08 PM UTC

    Hi @Erric 

    Unfortunately, Dual role device on H743 is not supported by current ST USB Middleware. 

    To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL