STM32H743 USB CDC HardFault
- 5 replies
- 431 views
Hi ST Community,
Our project uses STM32H743 (LQFP100). The system clock is set at the max 480MHz.
The USB Device interrupts would occasionally cause a HardFault. For example, if we plug in or unplug the USB.
The data hpcd would occasionally be 0xFFFFFFFF. Sometimes it's the hpcd->pClass[0]
We have enough size for the stack and heap.
A "workaround" is to lower the system clock to 240MHz...
What we don't understand is that the USB clock source is from the "RC48" 48MHz clock, independent from the system clock, which sources the HSE. How does lowering the system clock help resolve this issue? We also tried using HSE to generate the 48MHz for the USB, but the USB just doesn't run.
Is there other settings or configurations that we might have set incorrectly?
Another thing to mention is that we have a conflict with the RCC CRS SYNC.

Attached is our clock configuration and .ioc file for your reference.

Thanks in advance.