STM32H743 TCP-IP fault (FreeRTOS LwIP)
Hi all!
I'm trying to use LwIP stack on STM32H743XI.
I am installing a TCP-IP server. I use CubeMX for initialization. The ethernetif.c file is slightly edited to temporarily disable the d-cache in one of the I / O functions, as shown in one issue, this is an h-series problem.
In the beginning, I configure the MPU, initialize the stack by calling the MX_LWIP_Init () command.
Next, I create a connection by calling the netconn_new () command and
bind the structure to port # 502 with the netconn_bind () command.
Next, I specify the connection to listen for incoming connection requests with the netconn_listen () command.
Further, if a connection arrives, I create a new task in which I call netconn_accept () to block until we receive an incoming connection request.
Further, if netconn_accept () returned the value "ERR_OK", then I call netconn_recv () to accept the data.
If recv returns the value "ERR_OK", I enter the critical section,
call netbuf_data () to process the data and somehow process it,
destroy the received buffer with the netbuf_delete () command and
exit the critical section, then
return to the netconn_recv () function.
This works for a while, always different in time. It may fail quickly, maybe after 40 minutes. Reception is two messages with a length of 12 bytes each time per second. The causes of crashes can be different, but most often it is a hang when switching FreeRTOS tasks. There are also MemManageFault and HardFault. Sometimes a message arrives with the first 8 bytes zero (this is an abnormal situation, the request source (client) sends the correct data, I checked using WireShark).
I am using Keil uVision, the standard compiler of version 5. FreeRTOS v10.0.1, LwIP v2.0.3, CubeMX 5.3.0, service pack 1.4.0. I tried to install the latest version of LwIP, it did not help.
FreeRTOS works correctly if you do not open a TCP-IP connection. Ping works stably for a long time. The stack does not overflow, I checked it by displaying debugging information. vApplicationStackOverflowHook () is not called, but is in the code.
I ask for any help.
Thank!
err_t err, recv_err;
struct netconn *conn;
struct netbuf *inbuf;
struct netconn *newconn;
// receive incoming param
struct_sock *arg_sock;
arg_sock = (struct_sock*) argument;
conn = arg_sock->conn;
u16_t buflen;
static char* buf;
for(;;)
{
err = netconn_accept(conn, &newconn);
if (err == ERR_OK) {
while (1) {
recv_err = netconn_recv(newconn, &inbuf);
if (recv_err == ERR_OK) {
taskENTER_CRITICAL ();
netbuf_data(inbuf, (void**)&buf, &buflen);
...
...
...
netbuf_delete(inbuf);
taskEXIT_CRITICAL();
} else {
netbuf_delete(inbuf);
netconn_close(newconn);
netconn_delete(newconn);
break;
}
}
}
else
{
osDelay(100);
}
}MPU init:
void MPU_Config(void)
{
MPU_Region_InitTypeDef MPU_InitStruct = {0};
/* Disables the MPU */
HAL_MPU_Disable();
/** Initializes and configures the Region and the memory to be protected
*/
MPU_InitStruct.Enable = MPU_REGION_ENABLE;
MPU_InitStruct.Number = MPU_REGION_NUMBER0;
MPU_InitStruct.BaseAddress = 0x30040000;
MPU_InitStruct.Size = MPU_REGION_SIZE_16KB;
MPU_InitStruct.SubRegionDisable = 0x0;
MPU_InitStruct.TypeExtField = MPU_TEX_LEVEL1;
MPU_InitStruct.AccessPermission = MPU_REGION_FULL_ACCESS;
MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_ENABLE;
MPU_InitStruct.IsShareable = MPU_ACCESS_NOT_SHAREABLE;
MPU_InitStruct.IsCacheable = MPU_ACCESS_NOT_CACHEABLE;
MPU_InitStruct.IsBufferable = MPU_ACCESS_NOT_BUFFERABLE;
HAL_MPU_ConfigRegion(&MPU_InitStruct);
/** Initializes and configures the Region and the memory to be protected
*/
MPU_InitStruct.Enable = MPU_REGION_ENABLE;
MPU_InitStruct.Number = MPU_REGION_NUMBER1;
MPU_InitStruct.BaseAddress = 0x30044000;
MPU_InitStruct.Size = MPU_REGION_SIZE_16KB;
MPU_InitStruct.SubRegionDisable = 0x0;
MPU_InitStruct.TypeExtField = MPU_TEX_LEVEL0;
MPU_InitStruct.AccessPermission = MPU_REGION_FULL_ACCESS;
MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_ENABLE;
MPU_InitStruct.IsShareable = MPU_ACCESS_NOT_SHAREABLE;
MPU_InitStruct.IsCacheable = MPU_ACCESS_CACHEABLE;
MPU_InitStruct.IsBufferable = MPU_ACCESS_NOT_BUFFERABLE;
HAL_MPU_ConfigRegion(&MPU_InitStruct);
/** Initializes and configures the Region and the memory to be protected
*/
MPU_InitStruct.Enable = MPU_REGION_ENABLE;
MPU_InitStruct.Number = MPU_REGION_NUMBER2;
MPU_InitStruct.BaseAddress = 0x30040000;
MPU_InitStruct.Size = MPU_REGION_SIZE_256B;
MPU_InitStruct.SubRegionDisable = 0x0;
MPU_InitStruct.TypeExtField = MPU_TEX_LEVEL0;
MPU_InitStruct.AccessPermission = MPU_REGION_FULL_ACCESS;
MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_ENABLE;
MPU_InitStruct.IsShareable = MPU_ACCESS_NOT_SHAREABLE;
MPU_InitStruct.IsCacheable = MPU_ACCESS_NOT_CACHEABLE;
MPU_InitStruct.IsBufferable = MPU_ACCESS_BUFFERABLE;
HAL_MPU_ConfigRegion(&MPU_InitStruct);
/* Enables the MPU */
HAL_MPU_Enable(MPU_HFNMI_PRIVDEF);
}