Skip to main content
Associate
May 14, 2026
Question

STM32H743 Flash erase erases the wrong bank

Hi,

I am building a program that can flash new firmware onto a STM32H743ZIT6 via CAN. It does so by utilizing the dual bank feature and ping-ponging between bank 1 and bank 2. It receives the firmware via CAN and buffers it. Before writing it to the inactive bank it first erases said bank.

When running form bank 1 this works just fine and it is able to reboot to the newly flashed bank. When going from bank 2 back to bank 1 however, it encounters an issue. It crashes in the erase step and will not restart.

After I manually disable the SWAP_BANK bit using STM32CubeProgrammer it runs again on bank 1 without flashing again. This (I think) tells me it is deleting bank 2 while also running on it.

Attached you find the function in question, do you have any idea where i went wrong?

 

void foc_erase_inactive_bank() {
 // Determine inactive bank from SWAP_BANK bit
 uint8_t inactive_bank = (FLASH->OPTCR & FLASH_OPTCR_SWAP_BANK) ? 1 : 2;
 uint32_t bank_to_erase = (inactive_bank == 1) ? FLASH_BANK_1 : FLASH_BANK_2;

 LOG_INFO("FOC [ERASE] Starting mass erase of bank %u", inactive_bank);

 // unlock flash
 if (HAL_FLASH_Unlock() != HAL_OK) {
 LOG_ERROR("FOC [ERASE] HAL_FLASH_Unlock failed");
 foc.state = FOC_STATE_ERROR;
 return;
 }
 // Disable instruction cache prior to flash operation
 SCB_DisableICache();

 // Configure and execute mass erase
 FLASH_EraseInitTypeDef erase_init = {
 .TypeErase = FLASH_TYPEERASE_MASSERASE,
 .Banks = bank_to_erase,
 .VoltageRange = FLASH_VOLTAGE_RANGE_3,
 };

 uint32_t erase_error = 0U;
 HAL_StatusTypeDef erase_result = HAL_FLASHEx_Erase(&erase_init, &erase_error);

 // Re-enable cache and lock flash
 SCB_EnableICache();
 HAL_FLASH_Lock();

 // handle error
 if (erase_result != HAL_OK) {
 uint32_t hal_error = HAL_FLASH_GetError();
 LOG_ERROR(
 "FOC [ERASE] Mass erase failed with status %lu, HAL error: 0x%08X",
 (unsigned long)erase_result, hal_error);
 foc.state = FOC_STATE_ERROR;
 return;
 }

 LOG_INFO("FOC [ERASE] Successfully erased bank %u", inactive_bank);
}

 

3 replies

Pavel A.
May 14, 2026

Is this STM32H743ZIT6  ?

JoniAuthor
Associate
May 15, 2026

Yes, absolutely, i mistyped. It's the STM32H743ZIT6. Thanks!

ST Technical Moderator
May 15, 2026
In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om