Skip to main content
GTrin.2
Visitor II
Mar 21, 2023 12:12 PM UTC
Question

STM32H723VE Ethernet

Hello,

I'm using the STM32H723VE chip in my project and I'm having some difficulties getting the Ethernet interface fully functional. Used this chip with the KSZ8041 and I'm giving ping. I enabled the D-Cache and I-Cache, performed the MPU settings. I'm trying to implement the Modbus TCP protocol, I open and close the TCP connection, it works for a while and then it stops working and then it doesn't work anymore. I'm a few things on the forum, however nothing has yet worked.

I use STM32Cube FW_H7 V1.11.0 (6.8.0).

Some relevant settings:

**** __FLASH.id

 /* Modification start */

 .lwip_sec (NOLOAD) : {

 . = ABSOLUTE(0x30000000);

 *(.RxDecripSection) 

  

 . = ABSOLUTE(0x30000080);

 *(.TxDecripSection)

  

 . = ABSOLUTE(0x30000100);

 *(.Rx_PoolSection) 

 } >RAM_D2

 /* Modification end */

**** lwipopts.h

/* STM32CubeMX Specific Parameters (not defined in opt.h) ---------------------*/

/* Parameters set in STM32CubeMX LwIP Configuration GUI -*/

/*----- WITH_RTOS enabled (Since FREERTOS is set) -----*/

#define WITH_RTOS 1

/* Temporary workaround to avoid conflict on errno defined in STM32CubeIDE and lwip sys_arch.c errno */

#undef LWIP_PROVIDE_ERRNO

#define LWIP_ERRNO_STDINCLUDE

/*----- WITH_MBEDTLS enabled (Since MBEDTLS and FREERTOS are set) -----*/

#define WITH_MBEDTLS 0

/*----- CHECKSUM_BY_HARDWARE enabled -----*/

#define CHECKSUM_BY_HARDWARE 0

/*-----------------------------------------------------------------------------*/

/* LwIP Stack Parameters (modified compared to initialization value in opt.h) -*/

/* Parameters set in STM32CubeMX LwIP Configuration GUI -*/

/*----- Value in opt.h for LWIP_DHCP: 0 -----*/

#define LWIP_DHCP 1

/*----- Default value in ETH configuration GUI in CubeMx: 1524 -----*/

#define ETH_RX_BUFFER_SIZE 1536

/*----- Value in opt.h for LWIP_DNS: 0 -----*/

#define LWIP_DNS 0

/*----- Default Value for MEMP_NUM_UDP_PCB: 4 ---*/

#define MEMP_NUM_UDP_PCB 6

/*----- Default Value for MEMP_NUM_TCP_PCB: 5 ---*/

#define MEMP_NUM_TCP_PCB 8

/*----- Value in opt.h for MEM_ALIGNMENT: 1 -----*/

#define MEM_ALIGNMENT 4

/*----- Default Value for MEMP_NUM_NETCONN: 4 ---*/

#define MEMP_NUM_NETCONN 16

/*----- Default Value for MEM_SIZE: 1600 ---*/

#define MEM_SIZE 4*1024

/*----- Default Value for H7 devices: 0x30044000 -----*/

#define LWIP_RAM_HEAP_POINTER 0x30002000

/*----- Value supported for H7 devices: 1 -----*/

#define LWIP_SUPPORT_CUSTOM_PBUF 1

/*----- Value in opt.h for LWIP_ETHERNET: LWIP_ARP || PPPOE_SUPPORT -*/

#define LWIP_ETHERNET 1

/*----- Default Value for LWIP_RANDOMIZE_INITIAL_LOCAL_PORTS: 0 ---*/

#define LWIP_RANDOMIZE_INITIAL_LOCAL_PORTS 1

/*----- Default Value for LWIP_MULTICAST_TX_OPTIONS: 0 ---*/

#define LWIP_MULTICAST_TX_OPTIONS 1

/*----- Default Value for LWIP_DHCP_CHECK_LINK_UP: 0 ---*/

#define LWIP_DHCP_CHECK_LINK_UP 1

/*----- Value in opt.h for LWIP_DNS_SECURE: (LWIP_DNS_SECURE_RAND_XID | LWIP_DNS_SECURE_NO_MULTIPLE_OUTSTANDING | LWIP_DNS_SECURE_RAND_SRC_PORT) -*/

#define LWIP_DNS_SECURE 7

/*----- Default Value for TCP_MSS: 536 ---*/

#define TCP_MSS 1460

/*----- Value in opt.h for TCP_SND_QUEUELEN: (4*TCP_SND_BUF + (TCP_MSS - 1))/TCP_MSS -----*/

#define TCP_SND_QUEUELEN 9

/*----- Value in opt.h for TCP_SNDQUEUELOWAT: LWIP_MAX(TCP_SND_QUEUELEN)/2, 5) -*/

#define TCP_SNDQUEUELOWAT 5

/*----- Default Value for LWIP_NETIF_API: 0 ---*/

#define LWIP_NETIF_API 1

/*----- Default Value for LWIP_NETIF_STATUS_CALLBACK: 0 ---*/

#define LWIP_NETIF_STATUS_CALLBACK 1

/*----- Value in opt.h for LWIP_NETIF_LINK_CALLBACK: 0 -----*/

#define LWIP_NETIF_LINK_CALLBACK 1

 /*----- Default Value for LWIP_NETIF_STATUS_CALLBACK: 0 ---*/

 #define LWIP_NETIF_STATUS_CALLBACK 1

/*----- Value in opt.h for TCPIP_THREAD_STACKSIZE: 0 -----*/

#define TCPIP_THREAD_STACKSIZE 1024

/*----- Value in opt.h for TCPIP_THREAD_PRIO: 1 -----*/

#define TCPIP_THREAD_PRIO 24

/*----- Value in opt.h for TCPIP_MBOX_SIZE: 0 -----*/

#define TCPIP_MBOX_SIZE 6

/*----- Value in opt.h for SLIPIF_THREAD_STACKSIZE: 0 -----*/

#define SLIPIF_THREAD_STACKSIZE 1024

/*----- Value in opt.h for SLIPIF_THREAD_PRIO: 1 -----*/

#define SLIPIF_THREAD_PRIO 3

/*----- Value in opt.h for DEFAULT_THREAD_STACKSIZE: 0 -----*/

#define DEFAULT_THREAD_STACKSIZE 1024

/*----- Value in opt.h for DEFAULT_THREAD_PRIO: 1 -----*/

#define DEFAULT_THREAD_PRIO 3

/*----- Value in opt.h for DEFAULT_UDP_RECVMBOX_SIZE: 0 -----*/

#define DEFAULT_UDP_RECVMBOX_SIZE 6

/*----- Value in opt.h for DEFAULT_TCP_RECVMBOX_SIZE: 0 -----*/

#define DEFAULT_TCP_RECVMBOX_SIZE 6

/*----- Value in opt.h for DEFAULT_ACCEPTMBOX_SIZE: 0 -----*/

#define DEFAULT_ACCEPTMBOX_SIZE 6

/*----- Default Value for LWIP_SO_RCVTIMEO: 0 ---*/

#define LWIP_SO_RCVTIMEO 1

/*----- Value in opt.h for RECV_BUFSIZE_DEFAULT: INT_MAX -----*/

#define RECV_BUFSIZE_DEFAULT 2000000000

/*----- Value in opt.h for LWIP_USE_EXTERNAL_MBEDTLS: 0 -----*/

#define LWIP_USE_EXTERNAL_MBEDTLS 0

/*----- Default Value for LWIP_HTTPD: 0 ---*/

#define LWIP_HTTPD 0

/*----- Value in opt.h for HTTPD_USE_CUSTOM_FSDATA: 0 -----*/

#define HTTPD_USE_CUSTOM_FSDATA 0

/*----- Default Value for LWIP_SNTP: 0 ---*/

#define LWIP_SNTP 0

/*----- Default Value for LWIP_TFTP: 0 ---*/

#define LWIP_TFTP 0

/*----- Default Value for LWIP_STATS: 0 ---*/

#define LWIP_STATS 1

/*----- Value in opt.h for MIB2_STATS: 0 or SNMP_LWIP_MIB2 -----*/

#define MIB2_STATS 0

/*----- Value in opt.h for CHECKSUM_GEN_IP: 1 -----*/

#define CHECKSUM_GEN_IP 0

/*----- Value in opt.h for CHECKSUM_GEN_UDP: 1 -----*/

#define CHECKSUM_GEN_UDP 0

/*----- Value in opt.h for CHECKSUM_GEN_TCP: 1 -----*/

#define CHECKSUM_GEN_TCP 0

/*----- Value in opt.h for CHECKSUM_GEN_ICMP: 1 -----*/

#define CHECKSUM_GEN_ICMP 0

/*----- Value in opt.h for CHECKSUM_GEN_ICMP6: 1 -----*/

#define CHECKSUM_GEN_ICMP6 0

/*----- Value in opt.h for CHECKSUM_CHECK_IP: 1 -----*/

#define CHECKSUM_CHECK_IP 0

/*----- Value in opt.h for CHECKSUM_CHECK_UDP: 1 -----*/

#define CHECKSUM_CHECK_UDP 0

/*----- Value in opt.h for CHECKSUM_CHECK_TCP: 1 -----*/

#define CHECKSUM_CHECK_TCP 0

/*----- Value in opt.h for CHECKSUM_CHECK_ICMP: 1 -----*/

#define CHECKSUM_CHECK_ICMP 0

/*----- Value in opt.h for CHECKSUM_CHECK_ICMP6: 1 -----*/

#define CHECKSUM_CHECK_ICMP6 0

RX_POOL is coming in RAM_D2.

This topic has been closed for replies.

2 replies

KDJEM.1
ST Technical Moderator
Mar 22, 2023 7:30 AM UTC

Hello @GTrin.2​ ​ and welcome to the Community :),

Please follow this article "Ethernet not working on STM32H7x3", it may resolve your problem.

Also, I advise you, when you configurated the ethernet project, to get inspired form the steps described in this FAQ: How to create project for STM32H7 with Ethernet and LwIP stack working.

This FAQ will help you to configure your project in STM32CubeMX .

Also, you can get started with the example provided here STM32H7-LwIP-Examples.

I hope this help you!

Kaouthar

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.