Skip to main content
Visitor II
Nov 4, 2025 3:21 PM UTC
Question

STM32H723 PSSI DMA

Post edited by ST moderator to be inline with the community rules for the code sharing. In next time please use </> button to paste your code. Please read this post: How to insert source code.

Hello,  

i have a Project, where i have an FPGA connected to a STM32H723 via PSSI. The FPGA sends out 16 Bit of Dummy Data over 8 Data Lines Every 1 ms. In the STM i can receive the Data without using DMA like this: "HAL_PSSI_Receive(&hpssi,&received_pssi, 1, 5000)" 

Now i enabled DMA in CubeMX (DMA1 Stream 0). Inside the main.c Cube created " MX_DMA_Init();" for me. 

I added:

HAL_PSSI_ENABLE(&hpssi);

if (HAL_PSSI_Receive_DMA(&hpssi, (uint32_t*)rxBuffer, BUFFER_SIZE) != HAL_OK)
{
Error_Handler();
}
HAL_NVIC_EnableIRQ(DMA1_Stream0_IRQn);

And this does not end up in the Error Handler. 

 

As Soon as the main while loop is executed, i end up in the "HAL_PSSI_ErrorCallback" with the Error ID "0" (which corresponds to "HAL_PSSI_ERROR_NONE", so an Error with no Error? 

 

After that, the rxBuffer stays empty. So How do i correctly init a DMA for PSSI and then access the incoming Data? 

 

best Regards Karl 

1 reply

ST Technical Moderator
Nov 5, 2025 10:11 AM UTC

Hello @KarlHungus38 

Please refer to the example below to configure your DMA:

STM32CubeH7/Projects/NUCLEO-H7A3ZI-Q/Examples/PSSI/PSSI_Transmit_Receive_DMA at master · STMicroelectronics/STM32CubeH7

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om