Skip to main content
Associate
Dec 12, 2025 12:02 PM UTC
Question

STM32H7 sends USB NAK when data sent from host (PC)

Hi, 
I use STM32H7 with STCUBE 11.1.
I use RNDIS module  usbd_cdc_rndis.h to communicate with a PC.

Sometimes when the PC sends a frame the STM32 replies with NAK, here is the sequence that repeats:

SYNC
PID OUT
Address
CRC
EOP

SYNC
PID DATA0
data 30 bytes
CRC
EOP

SYNC
PID NAK
EOP

What might be the issue? Can I change the USB interval (CDC_RNDIS_FS_BINTERVAL)?


BR
Jonas



3 replies

ST Technical Moderator
Dec 15, 2025 10:34 AM UTC

Hi @Jonas_A 

NAK is a normal USB handshake response that tells the host "I am not ready to receive data right now, please retry later." not necessarily an issue.
Would you specify the issue in application layer ? Do you use reference board? H735 DK? Do you reproduce using the example firmware? 

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL
Jonas_AAuthor
Associate
Dec 16, 2025 12:32 PM UTC

When this happens the PC resends the USB frame infinitely because the STM32 always sends NAK.
Do you know how to troubleshoot this? I use a j-link so I can set breakpoints etc.,  do you know which function that set the reply to NAK?
The attached .csv file is a log from the logic analyzer that I use.
The first packet that is responded with a NAK starts on line 112095 (byte: 0x40)

waclawek.jan
Super User
Jul 7, 2026 10:10 AM UTC

As problem appears to be with OUT i.e. Host->Device, the way how this works is, that at the beginning (after enumeration) you enable given endpoint by setting OTG_DOEPCTLx.EPENA, and then, if needed, after receiving and processing one or more OUT packets (depending on OTG_DOEPTSIZx settings, see below) to this endpoint.

> Do you know how to troubleshoot this?

As always: observe registers’ content and memories/variables, trace the execution path. Formulate hypotheses, perform tests to confirm or reject these. You have to own the code, of course, whether by having it written yourself or by having it studied.

> do you know which function that set the reply to NAK

It’s not *function* but *hardware*,  (although some function *could* set it if needed, by setting OTG_DOEPCTLx.SNAK, or globally by setting OTG_DCTL.SGONAK). Hardware (documentation uses “core”) sets it when packets number/data size set in OTG_DOEPTSIZx is exhausted, FIFO for given endpoint is full, zero-length-packet is received from host; or maybe there are some other reasons, too.

JW