Skip to main content
Associate III
Feb 16, 2026 1:56 PM UTC
Solved

STM32H7 jump to application from bootloader

Hi everyone, I'm having trouble jumping to the app from the bootloader.
The application is located here, writing doesn't give me errors. So I assume the problem is Jump.

#define FLASH_USER_START_ADDR ADDR_FLASH_SECTOR_2_BANK1

 Il main del bootloader è costituito così

int main(void)
{
 /* USER CODE BEGIN 1 */
	
 /* USER CODE END 1 */

 /* MCU Configuration--------------------------------------------------------*/

 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();

 /* USER CODE BEGIN Init */

 /* USER CODE END Init */

 /* Configure the system clock */
 SystemClock_Config();

 /* USER CODE BEGIN SysInit */

 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_QUADSPI_Init();
 MX_SPI4_Init();
 MX_I2C1_Init();
 MX_RTC_Init();
 MX_FMC_Init();
 MX_USART6_UART_Init();
 /* USER CODE BEGIN 2 */
	HAL_GPIO_WritePin(ENABLE_3v3_WIFIPRINTER_uC_GPIO_Port, ENABLE_3v3_WIFIPRINTER_uC_Pin, GPIO_PIN_SET); 
	printf("\n\n*****START MAIN Bootloader *****\n\n");
	if (!USB_VBUS_Present())
 { 
		DebugApplicationHeader(); 
 JumpToUserApplication();
 }
.
.
.

With 

void DebugApplicationHeader(void)
{
	printf("\n=== APPLICATION HEADER DUMP ===\n");
	printf("Reading from: 0x%08lX\n", FLASH_USER_START_ADDR);
	uint32_t *app = (uint32_t*)FLASH_USER_START_ADDR; 
	// Primi 16 vettori
	for(int i = 0; i < 16; i++)
	{
		printf("[%2d] 0x%08lX: 0x%08lX", i, FLASH_USER_START_ADDR + (i*4), app[i]);
		// Aggiungi descrizione
		if(i == 0) printf(" <- Initial SP");
		else if(i == 1) printf(" <- Reset Handler");
		else if(i == 2) printf(" <- NMI");
		else if(i == 3) printf(" <- HardFault"); 
		printf("\n");
	} 
	// Verifica se � tutto 0xFF (flash vuota)
	bool isEmpty = true;
	for(int i = 0; i < 64; i++)
	{
		if(app[i] != 0xFFFFFFFF && app[i] != 0x00000000)
		{
			isEmpty = false;
			break;
		}
	} 
	if(isEmpty)
	{
		printf("\n WARNING: Flash appears empty or erased!\n");
	} 
	printf("================================\n\n");
}

void JumpToUserApplication(void)
{
	uint32_t appStack = *(__IO uint32_t*)FLASH_USER_START_ADDR;
	uint32_t appEntry = *(__IO uint32_t*)(FLASH_USER_START_ADDR + 4);
	
	// 1. Validazione
	if (((appStack & 0x2FF00000) != 0x20000000) && ((appStack & 0x2FF00000) != 0x24000000)) 
	{
		printf("ERROR: Invalid application at 0x%08lX\n", FLASH_USER_START_ADDR);
		return;
	}
	
	// 2. Debug
	printf("Jumping to application at 0x%08lX\n", FLASH_USER_START_ADDR);
	printf("SP: 0x%08lX, PC: 0x%08lX\n", appStack, appEntry);
	HAL_Delay(50);
	
	// 3. Disabilita interrupt
	printf("Disabling IRQ...\n");
	HAL_Delay(10);
	__disable_irq();
	printf("IRQ disabled\n"); // Questo potrebbe non stampare
	
	// 4. Disabilita SysTick
	printf("Disabling SysTick...\n");
	SysTick->CTRL = 0;
	SysTick->LOAD = 0;
	SysTick->VAL = 0;
	printf("SysTick disabled\n");
	
	// 5. Cache - PUNTO CRITICO
	printf("Disabling I-Cache...\n");
	SCB_DisableICache();
	printf("I-Cache disabled\n");
	
	printf("Disabling D-Cache...\n");
//	SCB_DisableDCache();
	printf("D-Cache disabled\n");
	
	printf("Invalidating I-Cache...\n");
	SCB_InvalidateICache();
	printf("I-Cache invalidated\n");
	
	printf("Invalidating D-Cache...\n");
//	SCB_InvalidateDCache();
	printf("D-Cache invalidated\n");
	
	// 6. MPU
	printf("Checking MPU...\n");
	if (SCB->SHCSR & SCB_SHCSR_MEMFAULTENA_Msk)
	{
		printf("Disabling MPU...\n");
		HAL_MPU_Disable();
		printf("MPU disabled\n");
	}
	else printf("MPU not active\n"); 
	// 7. NVIC
	printf("Clearing NVIC...\n");
	for (uint32_t i = 0; i < 8; i++)
	{
		NVIC->ICER[i] = 0xFFFFFFFF;
		NVIC->ICPR[i] = 0xFFFFFFFF;
	}
	printf("NVIC cleared\n");
	
	// 8. Deinit periferiche
//	printf("Deinit UART...\n");
	HAL_UART_DeInit(&huart6);
	HAL_SPI_DeInit(&hspi4);
	HAL_QSPI_DeInit(&hqspi);
	HAL_I2C_DeInit(&hi2c1);
	HAL_RTC_DeInit(&hrtc);
	HAL_SDRAM_DeInit(&hsdram1);
	// Dopo questo punto le printf non funzioneranno pi�!
	
	// 9. HAL Deinit
	HAL_DeInit(); 
//	printf("Hal DeInit\n");
	// 10. VTOR
	SCB->VTOR = FLASH_USER_START_ADDR; 
//	printf("VTOR \n");
	// 11. MSP
	__set_MSP(appStack); 
//	printf("MSP\n"); 
	// 12. Control
	__set_CONTROL(0); 
//	printf("CONTROL\n");
	// 13. Barriere
	__DSB();
//	printf("DSB\n");
	__ISB(); 
	// 14. JUMP!
//	printf("Pre JUMP\n");
	JumpToApplication = (pFunction)appEntry;
//	printf("JUMP\n");
	JumpToApplication(); 
//	printf("After Jump\n");
}

 these are the prints instead

=== APPLICATION HEADER DUMP ===
Reading from: 0x08040000
[ 0] 0x08040000: 0x24064AB8 <- Initial SP
[ 1] 0x08040004: 0x08040371 <- Reset Handler
[ 2] 0x08040008: 0x0804B49D <- NMI
[ 3] 0x0804000C: 0x08048AEB <- HardFault
[ 4] 0x08040010: 0x0804B0AD
[ 5] 0x08040014: 0x08042105
[ 6] 0x08040018: 0x08050D29
[ 7] 0x0804001C: 0x00000000
[ 8] 0x08040020: 0x00000000
[ 9] 0x08040024: 0x00000000
[10] 0x08040028: 0x00000000
[11] 0x0804002C: 0x080402B1
[12] 0x08040030: 0x080427CD
[13] 0x08040034: 0x00000000
[14] 0x08040038: 0x0804030D
[15] 0x0804003C: 0x0804E0E5
================================

Jumping to application at 0x08040000
SP: 0x24064AB8, PC: 0x08040371
Disabling IRQ...
IRQ disabled
Disabling SysTick...
SysTick disabled
Disabling I-Cache...
I-Cache disabled
Disabling D-Cache...
D-Cache disabled
Invalidating I-Cache...
I-Cache invalidated
Invalidating D-Cache...
D-Cache invalidated
Checking MPU...
MPU not active
Clearing NVIC...
NVIC cleared

How can I correct this?

Giovanni3Best answer
Associate III
Feb 16, 2026 4:07 PM UTC

I solved it by moving the application start to sector 3 (0x08060000)

3 replies

mƎALLEm
ST Technical Moderator
Feb 16, 2026 3:07 PM UTC
To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Giovanni3Author
Associate III
Feb 16, 2026 3:36 PM UTC

Thanks for the reply, Meallem, but the shared thread mentions the application jump at bootloader. I need the opposite. I also added that I previously had to port from SMT32F7 to STm32H7. On the SMT32F7, I managed the application jump the same way, and it worked. Are there things that need to be implemented differently?
I use the same strategy to jump to the application on the SMT32L4, and I'm having no problems.

Giovanni3AuthorBest answer
Associate III
Feb 16, 2026 4:07 PM UTC

I solved it by moving the application start to sector 3 (0x08060000)