Skip to main content
yuri CH
Senior
Jul 26, 2021 10:26 AM UTC
Question

STM32H7 firmware updgrade using ethernet

Hello!

I am currently working on a project using the stm32h74.

In previous projects i have used this mechanism using UART or SPI but never ethernet.

Trying to understand wether it is possible to use the built in stm32 bootloader using ethernet?

Thanks :)

This topic has been closed for replies.

4 replies

TDK
Jul 26, 2021 1:27 PM UTC

> Trying to understand wether it is possible to use the built in stm32 bootloader using ethernet?

It is not possible to use ethernet with the built-in bootloader. You would need to create your own.

"If you feel a post has answered your question, please click ""Accept as Solution""."
yuri CH
yuri CHAuthor
Senior
Jul 26, 2021 1:28 PM UTC

thanks ,

Are there any standard examples for this i can use?

Pavel A.
Jul 26, 2021 3:38 PM UTC

If TFTP is good for you, there are TFTP examples with LwIP.

With suitable host side software it even can be done with "raw ethernet", that's the target even can omit ARP support.

--pa