Skip to main content
MarkoSeverin
Visitor II
Jun 21, 2021 12:24 PM UTC
Solved

STM32H7 Ethernet Destination MAC address

Hi Guys,

I'm trying to do basic communication via Ethernet on a Nucleo H723 board. I would just like to send and receive a few Layer 2 frames. I'm going through the reference manual and the ETH HAL files to learn how the ethernet peripheral works. What I fail to understand so far is, where do you set the destination MAC for the packet which is to be transmitted? The source MAC is set in the ETH_MACA0HR and ETH_MACA0LR registers, great. The destination MAC address should be set on per-frame level, but the Transmit Descriptors do not contain any destination MAC address fields.

Can anyone give me a hint, as to how/where do you set the destination MAC address when sending a frame?

Regards,

Marko

This topic has been closed for replies.
Walid ZRELLI
Walid ZRELLIBest answer
Visitor II
Jun 29, 2021 2:35 PM UTC

Hello @MarkoSeverin​ ,

Welcome to ST Community :)

I recommend you to take a look at the applications provided under the H7 Firmware Package ( Firmware\Projects\NUCLEO-H723ZG\Applications\LwIP ).

Otherwise, take a look at this reference. It might be helpful.

BeST Regards,

Walid

2 replies

Walid ZRELLI
Walid ZRELLIBest answer
Visitor II
Jun 29, 2021 2:35 PM UTC

Hello @MarkoSeverin​ ,

Welcome to ST Community :)

I recommend you to take a look at the applications provided under the H7 Firmware Package ( Firmware\Projects\NUCLEO-H723ZG\Applications\LwIP ).

Otherwise, take a look at this reference. It might be helpful.

BeST Regards,

Walid

Pavel A.
Jun 29, 2021 9:41 PM UTC

>  The destination MAC address should be set on per-frame level, but the Transmit Descriptors do not contain any destination MAC address fields.

How about setting it right in the packet data? (and remember that you can assemble a packet from several buffers).