Associate III
March 5, 2026
Solved
STM32H533 and CubeMX generated project for CubeIDE
- 16 replies
- 909 views
Hello,
all my tools are updated to last ones, and software packages too.
I start an empty project using X Cube FreeRtos 1.5 (just a default task).
Play the soft with debug, and after a few seconds, press "Suspend" button to break the running program.
Then, there are a lot of calls to vPortSetupTimerInterrupt function (port.c) in the call stack.
The tick is by default 1ms and cpu clock to 250Mhz.
Not sure that is normal?
thanks for your help
Laurent