Skip to main content
Visitor II
Jul 18, 2025 2:33 AM UTC
Question

STM32H523HEYX flash write issue

STM32H523HEYX Flash Write Issue

1.
I’m currently working on a project using the STM32H523HEYX.
I'm using STM32CubeIDE, and the firmware libraries are up to date.
I’m also using STM32 X-CUBE-FREERTOS.

I’m trying to write data to Flash memory using the following functions:


2. HAL_FLASHEx_Erase(...);
HAL_FLASH_Program(FLASH_TYPEPROGRAM_QUADWORD, ASDF, (uint32_t)&quadData[0]);
However, the code triggers a HardFault when executed.

3. When I run the same code on a STM32H533 Nucleo board, it works without any fault and writes to Flash successfully.

4. I'm not sure why this Flash issue only occurs on the STM32H523HEYX.
If anyone has experienced a similar issue or knows of any related problems, I’d appreciate your advice.

Thank you, fellow developers!

This topic has been closed for replies.

1 reply

ST Technical Moderator
Jul 18, 2025 9:23 AM UTC

Hello @yb25Kim 

Please check the article below to debug your hard fault:

How to debug a HardFault on an Arm® Cortex®-M STM3... - STMicroelectronics Community

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om