Skip to main content
Associate
Dec 20, 2024 10:19 AM UTC
Solved

STM32H523 USB HOST WITHOUT EXTERNAL CRYSTAL

i am using stm32h523 mcu and using usb host msc feature for data logger. i generate code using cubemx and compiler keil. i want to know can i use usb host msc without external cyrstal  

This topic has been closed for replies.
mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Dec 20, 2024 11:59 AM UTC

Hello @PALGAU007 and welcome to the community,

Yes you can use HSI48 as source clock for USB on STM3232H523 MCU and no need for external crystal.

Hope that answers your question (if it's the case please accept as solution)

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

1 reply

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Dec 20, 2024 11:59 AM UTC

Hello @PALGAU007 and welcome to the community,

Yes you can use HSI48 as source clock for USB on STM3232H523 MCU and no need for external crystal.

Hope that answers your question (if it's the case please accept as solution)

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.