Skip to main content
hijax_pl
Associate III
Nov 27, 2024 12:28 PM UTC
Question

STM32H503 SVD / RM ADC_CFGR_EXTSEL logical error?

ADC_CFGR register and EXTSEL field.

In SVD this single field is split among four 1-bit long ones (according to RM0492) and enumerated values desciptions are messed up (adc_ext_trg0 & adc_ext_trg1 repeated for all 4 "subfields")

RM0492 discusses this as single field, which is correct, i.e.

"Bits 9:5 EXTSEL[4:0]: External trigger selection for regular group

These bits select the external event used to trigger the start of conversion of a regular group:
00000: adc_ext_trg0
00001: adc_ext_trg1
00010: adc_ext_trg2
00011: adc_ext_trg3
00100: adc_ext_trg4
00101: adc_ext_trg5
00110: adc_ext_trg6
00111: adc_ext_trg7
...
11111: adc_ext_trg31"

etc...

In the same time ADC_JSQR_JEXTSEL is defined as single 5-bit long field.

Bits 6:2 JEXTSEL[4:0]: External Trigger Selection for injected group

Logical inconsistecy...

Is SVD created from RM or vice versa?

Either way I think RM0492 (page 579), SVD and stm32h503xx.h files shall be corrected, to have both descriptions, i.e. EXTSEL & JEXTSEL aligned.

This topic has been closed for replies.

2 replies

ST Technical Moderator
Nov 27, 2024 3:16 PM UTC

Hello @hijax_pl,

Thank you again for having reported the point related to SVD issue.

I escalated this request internally for fix within the internal ticket number: 197196 (this tracking number is only for reference, not available outside of ST).

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
ST Technical Moderator
Dec 23, 2024 1:14 PM UTC

Hello @hijax_pl ,

The fix has been applied to the SVD files for STM32H5.
The new SVD files are available in the attached file.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks