Skip to main content
Explorer
Sep 30, 2026 5:50 PM UTC
Question

STM32H503 FLASH_ECCDETR incorrect OTP ADDR_ECC min value?

I have been writing some code to recover from the NMI after reading unwritten OTP addresses but I found a bit of a snag when checking that the Address listed in FLASH_ECCDETR is what I would expect after a read.

The Table 42 of the H503 reference manual (RM0492 Rev 2) lists a minimum ADDR_ECC offset of 0x0600. I was a little unsure what exactly this meant but `HAL_FLASHEx_GetEccInfo()` clearly runs:

// FLASH_ADDRESS_OFFSET_OTP is defined as 0x600 as you would expect here
pData->Address = (FLASH_OTP_BASE + ((addr_reg - FLASH_ADDRESS_OFFSET_OTP) * 4U)) & 0xFFFFFFFFU;

Seems simple enough then - the number is just which OTP word triggered the error minus 0x600.
Except the actual offset I am seeing in the address field is 0x200 instead of 0x600.

Reading an unwritten OTP at 0x08FFF010 gives me an ADDR_ECC of 0x204, reading 0x08FFF020 gives me 0x208, and so on...

Is this an error in the Reference Manual and HAL? Should the listed value be 0x200 or am I missing something here?

 

Thanks!

1 reply

ST Technical Moderator
Oct 12, 2026 3:29 PM UTC

Hello ​@Sergio_PDhe_DL 

I reported the issue internally.

Internal ticket number: CDM0066522 (This is an internal tracking number and is not accessible or usable by customers).

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om