Skip to main content
Associate II
Jan 13, 2026 5:18 AM UTC
Solved

Stm32H5 MPU Configuration for checking nullpointer access

Hello community members, 

I am using a STM32H5 with acitvated MPU region. I want to check and test dection of nullpointer access.

Because of safety reasons. I have configured and activated the mpu so far. When doing a write access to the declared null pointer, the MemManageFault Handler is called as expected. 

uint32_t *m_pTest = nullptr;

*m_pTest = m_value; // -> MemManageHandler is called (as expected)

when doing a read access, the BusFaulthandler is called

m_value = *m_pTest; // ->BusFaultHandler is called (not my expectation)

//here my mpu configuration and settings

SCB->SHCSR |= SCB_SHCSR_MEMFAULTENA_Msk |

SCB_SHCSR_BUSFAULTENA_Msk |

SCB_SHCSR_USGFAULTENA_Msk;

/* Configure the MPU to prevent NULL-pointer dereferencing ... */

//check nullpointer access Region1

MPU_InitStruct.Enable = MPU_REGION_ENABLE;

MPU_InitStruct.Number = MPU_REGION_NUMBER1;

MPU_InitStruct.BaseAddress = 0x00U;

MPU_InitStruct.LimitAddress = 0x200U;//512Byte for example

MPU_InitStruct.AttributesIndex = MPU_ATTRIBUTES_NUMBER1;

MPU_InitStruct.AccessPermission = MPU_REGION_PRIV_RO;

MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_DISABLE;

MPU_InitStruct.IsShareable = MPU_ACCESS_NOT_SHAREABLE;

HAL_MPU_ConfigRegion(&MPU_InitStruct);

 

MPU_AttributesInit.Number = MPU_ATTRIBUTES_NUMBER1;

MPU_AttributesInit.Attributes = MPU_DEVICE_nGnRnE | MPU_NOT_CACHEABLE

| MPU_TRANSIENT | MPU_NO_ALLOCATE;

HAL_MPU_ConfigMemoryAttributes(&MPU_AttributesInit);

 

/* Enables the MPU */

HAL_MPU_Enable(static_cast<uint32_t>(MPU_PRIVILEGED_DEFAULT));

 

////////////////////////

My question is:

can I configure MPU, that either a read or a write access to a nullpointer

the MemoryManagementFault - Handler is called ? Maybe changing of parameter:

AccessPermission, DisableExec, IsShareable, MPU_AttributesInit.Attributes

 

Many thansk in advance for your help.

Best regards

jhoerd

 

 

Khaled_DHIFBest answer
ST Employee
Jan 26, 2026 12:56 PM UTC

Hello @jhoerd ,

On this STM32H5, the behavior comes directly from what NULL is and how the H5 memory map looks.

In the toolchain, NULL ends up as a ((void *)0) in C, so a null pointer dereference is literally an access to address 0x00000000. On STM32H5, that address is in the External memories remap region in the memory map – it’s not internal Flash or SRAM, it’s an external/aliased bus region.

When you do:

uint32_t *p = NULL;
g_value = *p; // read from 0x00000000

the core issues a read to 0x00000000 on that external‑remap bus path. That access fails at the bus/memory level, so the CPU reports a BusFault. The fault is raised by the bus interface, not by the MPU permission logic.

On other STM32 ARMv8‑M parts, the same code will not give a BusFault if 0x00000000 is mapped differently (for example to an internal Flash alias).

And when you run as a Non‑Secure image with TrustZone enabled, a null dereference can also be classified as a SecureFault rather than MemManage.

kind regards,

"Please mark my answer as best by clicking on the “Accept as solution"" button if it fully answered your question. This will help other users find this solution faster.​"

2 replies

Khaled_DHIFBest answer
ST Employee
Jan 26, 2026 12:56 PM UTC

Hello @jhoerd ,

On this STM32H5, the behavior comes directly from what NULL is and how the H5 memory map looks.

In the toolchain, NULL ends up as a ((void *)0) in C, so a null pointer dereference is literally an access to address 0x00000000. On STM32H5, that address is in the External memories remap region in the memory map – it’s not internal Flash or SRAM, it’s an external/aliased bus region.

When you do:

uint32_t *p = NULL;
g_value = *p; // read from 0x00000000

the core issues a read to 0x00000000 on that external‑remap bus path. That access fails at the bus/memory level, so the CPU reports a BusFault. The fault is raised by the bus interface, not by the MPU permission logic.

On other STM32 ARMv8‑M parts, the same code will not give a BusFault if 0x00000000 is mapped differently (for example to an internal Flash alias).

And when you run as a Non‑Secure image with TrustZone enabled, a null dereference can also be classified as a SecureFault rather than MemManage.

kind regards,

"Please mark my answer as best by clicking on the “Accept as solution"" button if it fully answered your question. This will help other users find this solution faster.​"
jhoerdAuthor
Associate II
Jan 27, 2026 6:33 AM UTC

Hello Khaled_DHIF

many thanks for your answer. You helped me to undertand what happens in my test cases.

Best regards

jhoerd