Skip to main content
Associate III
June 27, 2026
Question

stm32h5 fat12 implemented, using eeprm as msc, issue is i2c is blocking superloop.

  • June 27, 2026
  • 2 replies
  • 74 views

 

Hi ,

 

Subject: i need to reduce the log write time what to do 

I have an STM32H503 logging ~20 bytes per line (HH:MM:SS , X.X) to a 24Cxx EEPROM over I2C @ 400 kHz, with FAT12 + USB MSC.

Blocking time = the main loop stalls ~100–200 ms on each append while EEPROM writes finish.

Each line only adds ~20 B of text, but my FAT code does full 512 B sector read-modify-write on the data sector, again on the root directory (file size), plus metadata read/write.

That’s ~1 KB+ programmed per line (many 64 B page programs), so EEPROM ACK/program time dominates — not the 20 B payload or I2C speed alone.

Basic issue: small appends through sector-based FAT on page EEPROM → huge writes per line.

I’m thinking: defer root/meta to session end (back button), RAM cache, write only dirty 64 B pages.

Is that the right fix? Can others get ~20–50 ms/line on 24Cxx without dropping FAT?

2 replies

Andrew Neil
Super User
June 27, 2026

This seems to be a duplicate of your existing thread:

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Pavel A.
June 27, 2026

What to do? Cache the current “block” of the MSC volume, compare and write only changed bytes. If the metadata updates affect the file modification time - drop or delay these updates.