Skip to main content
Associate
August 14, 2024
Question

STM32H5 External interrupt is not triggering

Hello there!

It would be really great if someone can look into this.

I even tested it by reading the state of the pin and the MCU detected when the button was pressed, however when I set it up to use EXTI, its not detecting the interrupt. Could there be something wrong with the IC?

Any help would be greatly appreciated.

 

 

 

/* USER CODE BEGIN Header */
/**
 ******************************************************************************
 * @file : main.c
 * @brief : Main program body
 ******************************************************************************
 * @attention
 *
 * Copyright (c) 2024 STMicroelectronics.
 * All rights reserved.
 *
 * This software is licensed under terms that can be found in the LICENSE file
 * in the root directory of this software component.
 * If no LICENSE file comes with this software, it is provided AS-IS.
 *
 ******************************************************************************
 */
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"

/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */

/* USER CODE END Includes */

/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */

/* USER CODE END PTD */

/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */

/* USER CODE END PD */

/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */

/* USER CODE END PM */

/* Private variables ---------------------------------------------------------*/
ADC_HandleTypeDef hadc1;

DAC_HandleTypeDef hdac1;

I2C_HandleTypeDef hi2c1;
I2C_HandleTypeDef hi2c2;

SPI_HandleTypeDef hspi1;

TIM_HandleTypeDef htim2;
TIM_HandleTypeDef htim3;

USART_HandleTypeDef husart3;

PCD_HandleTypeDef hpcd_USB_DRD_FS;

/* USER CODE BEGIN PV */

/* USER CODE END PV */

/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_ADC1_Init(void);
static void MX_DAC1_Init(void);
static void MX_I2C1_Init(void);
static void MX_SAU_Init(void);
static void MX_SPI1_Init(void);
static void MX_TIM2_Init(void);
static void MX_TIM3_Init(void);
static void MX_USB_PCD_Init(void);
static void MX_I2C2_Init(void);
static void MX_USART3_Init(void);
static void MX_ICACHE_Init(void);
/* USER CODE BEGIN PFP */

/* USER CODE END PFP */

/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
uint8_t bpin = 0;
/* USER CODE END 0 */

/**
 * @brief The application entry point.
 * @retval int
 */
int main(void)
{

 /* USER CODE BEGIN 1 */

 /* USER CODE END 1 */

 /* MCU Configuration--------------------------------------------------------*/

 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();

 /* USER CODE BEGIN Init */

 /* USER CODE END Init */

 /* Configure the system clock */
 SystemClock_Config();

 /* USER CODE BEGIN SysInit */

 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_ADC1_Init();
 MX_DAC1_Init();
 MX_I2C1_Init();
 MX_SAU_Init();
 MX_SPI1_Init();
 MX_TIM2_Init();
 MX_TIM3_Init();
 MX_USB_PCD_Init();
 MX_I2C2_Init();
 MX_USART3_Init();
 MX_ICACHE_Init();
 /* USER CODE BEGIN 2 */

 /* USER CODE END 2 */

 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 while (1)
 {
 /* USER CODE END WHILE */
	 //HAL_GPIO_ReadPin(GPIOC,Button_Pin)

		 if (HAL_GPIO_ReadPin(GPIOC,Button_Pin) == 0)
		 {
			 HAL_GPIO_WritePin(GPIOC, GPIO_PIN_10, GPIO_PIN_SET);
		 }
		 else
		 {
			 HAL_GPIO_WritePin(GPIOC, GPIO_PIN_10, GPIO_PIN_RESET);
		 }
		}

 /* USER CODE BEGIN 3 */
 }
 /* USER CODE END 3 */


/**
 * @brief System Clock Configuration
 * @retval None
 */
void SystemClock_Config(void)
{
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

 /** Configure the main internal regulator output voltage
 */
 __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE3);

 while(!__HAL_PWR_GET_FLAG(PWR_FLAG_VOSRDY)) {}

 /** Initializes the RCC Oscillators according to the specified parameters
 * in the RCC_OscInitTypeDef structure.
 */
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI48|RCC_OSCILLATORTYPE_HSI
 |RCC_OSCILLATORTYPE_LSI|RCC_OSCILLATORTYPE_CSI;
 RCC_OscInitStruct.HSIState = RCC_HSI_ON;
 RCC_OscInitStruct.HSIDiv = RCC_HSI_DIV2;
 RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
 RCC_OscInitStruct.LSIState = RCC_LSI_ON;
 RCC_OscInitStruct.HSI48State = RCC_HSI48_ON;
 RCC_OscInitStruct.CSIState = RCC_CSI_ON;
 RCC_OscInitStruct.CSICalibrationValue = RCC_CSICALIBRATION_DEFAULT;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
 RCC_OscInitStruct.PLL.PLLSource = RCC_PLL1_SOURCE_CSI;
 RCC_OscInitStruct.PLL.PLLM = 1;
 RCC_OscInitStruct.PLL.PLLN = 32;
 RCC_OscInitStruct.PLL.PLLP = 2;
 RCC_OscInitStruct.PLL.PLLQ = 2;
 RCC_OscInitStruct.PLL.PLLR = 2;
 RCC_OscInitStruct.PLL.PLLRGE = RCC_PLL1_VCIRANGE_2;
 RCC_OscInitStruct.PLL.PLLVCOSEL = RCC_PLL1_VCORANGE_WIDE;
 RCC_OscInitStruct.PLL.PLLFRACN = 0;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }

 /** Initializes the CPU, AHB and APB buses clocks
 */
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
 |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2
 |RCC_CLOCKTYPE_PCLK3;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSI;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
 RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
 RCC_ClkInitStruct.APB3CLKDivider = RCC_HCLK_DIV1;

 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_1) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure the programming delay
 */
 __HAL_FLASH_SET_PROGRAM_DELAY(FLASH_PROGRAMMING_DELAY_0);
}

/**
 * @brief ADC1 Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_ADC1_Init(void)
{

 /* USER CODE BEGIN ADC1_Init 0 */

 /* USER CODE END ADC1_Init 0 */

 ADC_ChannelConfTypeDef sConfig = {0};

 /* USER CODE BEGIN ADC1_Init 1 */

 /* USER CODE END ADC1_Init 1 */

 /** Common config
 */
 hadc1.Instance = ADC1;
 hadc1.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV1;
 hadc1.Init.Resolution = ADC_RESOLUTION_12B;
 hadc1.Init.DataAlign = ADC_DATAALIGN_RIGHT;
 hadc1.Init.ScanConvMode = ADC_SCAN_DISABLE;
 hadc1.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
 hadc1.Init.LowPowerAutoWait = DISABLE;
 hadc1.Init.ContinuousConvMode = DISABLE;
 hadc1.Init.NbrOfConversion = 1;
 hadc1.Init.DiscontinuousConvMode = DISABLE;
 hadc1.Init.ExternalTrigConv = ADC_SOFTWARE_START;
 hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;
 hadc1.Init.DMAContinuousRequests = DISABLE;
 hadc1.Init.SamplingMode = ADC_SAMPLING_MODE_NORMAL;
 hadc1.Init.Overrun = ADC_OVR_DATA_PRESERVED;
 hadc1.Init.OversamplingMode = DISABLE;
 if (HAL_ADC_Init(&hadc1) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure Regular Channel
 */
 sConfig.Channel = ADC_CHANNEL_1;
 sConfig.Rank = ADC_REGULAR_RANK_1;
 sConfig.SamplingTime = ADC_SAMPLETIME_2CYCLES_5;
 sConfig.SingleDiff = ADC_SINGLE_ENDED;
 sConfig.OffsetNumber = ADC_OFFSET_NONE;
 sConfig.Offset = 0;
 if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN ADC1_Init 2 */

 /* USER CODE END ADC1_Init 2 */

}

/**
 * @brief DAC1 Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_DAC1_Init(void)
{

 /* USER CODE BEGIN DAC1_Init 0 */

 /* USER CODE END DAC1_Init 0 */

 DAC_ChannelConfTypeDef sConfig = {0};

 /* USER CODE BEGIN DAC1_Init 1 */

 /* USER CODE END DAC1_Init 1 */

 /** DAC Initialization
 */
 hdac1.Instance = DAC1;
 if (HAL_DAC_Init(&hdac1) != HAL_OK)
 {
 Error_Handler();
 }

 /** DAC channel OUT1 config
 */
 sConfig.DAC_HighFrequency = DAC_HIGH_FREQUENCY_INTERFACE_MODE_DISABLE;
 sConfig.DAC_DMADoubleDataMode = DISABLE;
 sConfig.DAC_SignedFormat = DISABLE;
 sConfig.DAC_SampleAndHold = DAC_SAMPLEANDHOLD_DISABLE;
 sConfig.DAC_Trigger = DAC_TRIGGER_NONE;
 sConfig.DAC_OutputBuffer = DAC_OUTPUTBUFFER_ENABLE;
 sConfig.DAC_ConnectOnChipPeripheral = DAC_CHIPCONNECT_EXTERNAL;
 sConfig.DAC_UserTrimming = DAC_TRIMMING_FACTORY;
 if (HAL_DAC_ConfigChannel(&hdac1, &sConfig, DAC_CHANNEL_1) != HAL_OK)
 {
 Error_Handler();
 }

 /** DAC channel OUT2 config
 */
 if (HAL_DAC_ConfigChannel(&hdac1, &sConfig, DAC_CHANNEL_2) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN DAC1_Init 2 */

 /* USER CODE END DAC1_Init 2 */

}

/**
 * @brief I2C1 Initialization Function
 * @PAram None
 * @retval None
 */

/**
 * @brief I2C2 Initialization Function
 * @PAram None
 * @retval None
 */

/**
 * @brief ICACHE Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_ICACHE_Init(void)
{

 /* USER CODE BEGIN ICACHE_Init 0 */

 /* USER CODE END ICACHE_Init 0 */

 /* USER CODE BEGIN ICACHE_Init 1 */

 /* USER CODE END ICACHE_Init 1 */

 /** Enable instruction cache in 1-way (direct mapped cache)
 */
 if (HAL_ICACHE_ConfigAssociativityMode(ICACHE_1WAY) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_ICACHE_Enable() != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN ICACHE_Init 2 */

 /* USER CODE END ICACHE_Init 2 */

}

/**
 * @brief SAU Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_SAU_Init(void)
{

 /* USER CODE BEGIN SAU_Init 0 */

 /* USER CODE END SAU_Init 0 */

 /* USER CODE BEGIN SAU_Init 1 */

 /* USER CODE END SAU_Init 1 */
 /* USER CODE BEGIN SAU_Init 2 */

 /* USER CODE END SAU_Init 2 */

}

/**
 * @brief SPI1 Initialization Function
 * @PAram None
 * @retval None
 */


/**
 * @brief TIM2 Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_TIM2_Init(void)
{

 /* USER CODE BEGIN TIM2_Init 0 */

 /* USER CODE END TIM2_Init 0 */

 TIM_MasterConfigTypeDef sMasterConfig = {0};
 TIM_OC_InitTypeDef sConfigOC = {0};

 /* USER CODE BEGIN TIM2_Init 1 */

 /* USER CODE END TIM2_Init 1 */
 htim2.Instance = TIM2;
 htim2.Init.Prescaler = 32-1;
 htim2.Init.CounterMode = TIM_COUNTERMODE_UP;
 htim2.Init.Period = 25;
 htim2.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
 htim2.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_ENABLE;
 if (HAL_TIM_PWM_Init(&htim2) != HAL_OK)
 {
 Error_Handler();
 }
 sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;
 sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
 if (HAL_TIMEx_MasterConfigSynchronization(&htim2, &sMasterConfig) != HAL_OK)
 {
 Error_Handler();
 }
 sConfigOC.OCMode = TIM_OCMODE_PWM1;
 sConfigOC.Pulse = 0;
 sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH;
 sConfigOC.OCFastMode = TIM_OCFAST_DISABLE;
 if (HAL_TIM_PWM_ConfigChannel(&htim2, &sConfigOC, TIM_CHANNEL_1) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN TIM2_Init 2 */

 /* USER CODE END TIM2_Init 2 */
 HAL_TIM_MspPostInit(&htim2);

}

/**
 * @brief TIM3 Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_TIM3_Init(void)
{

 /* USER CODE BEGIN TIM3_Init 0 */

 /* USER CODE END TIM3_Init 0 */

 TIM_MasterConfigTypeDef sMasterConfig = {0};
 TIM_OC_InitTypeDef sConfigOC = {0};

 /* USER CODE BEGIN TIM3_Init 1 */

 /* USER CODE END TIM3_Init 1 */
 htim3.Instance = TIM3;
 htim3.Init.Prescaler = 12-1;
 htim3.Init.CounterMode = TIM_COUNTERMODE_UP;
 htim3.Init.Period = 9;
 htim3.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
 htim3.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_ENABLE;
 if (HAL_TIM_PWM_Init(&htim3) != HAL_OK)
 {
 Error_Handler();
 }
 sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;
 sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
 if (HAL_TIMEx_MasterConfigSynchronization(&htim3, &sMasterConfig) != HAL_OK)
 {
 Error_Handler();
 }
 sConfigOC.OCMode = TIM_OCMODE_PWM1;
 sConfigOC.Pulse = 0;
 sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH;
 sConfigOC.OCFastMode = TIM_OCFAST_DISABLE;
 if (HAL_TIM_PWM_ConfigChannel(&htim3, &sConfigOC, TIM_CHANNEL_1) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN TIM3_Init 2 */

 /* USER CODE END TIM3_Init 2 */
 HAL_TIM_MspPostInit(&htim3);

}

/**
 * @brief USART3 Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_USART3_Init(void)
{

 /* USER CODE BEGIN USART3_Init 0 */

 /* USER CODE END USART3_Init 0 */

 /* USER CODE BEGIN USART3_Init 1 */

 /* USER CODE END USART3_Init 1 */
 husart3.Instance = USART3;
 husart3.Init.BaudRate = 115200;
 husart3.Init.WordLength = USART_WORDLENGTH_8B;
 husart3.Init.StopBits = USART_STOPBITS_1;
 husart3.Init.Parity = USART_PARITY_NONE;
 husart3.Init.Mode = USART_MODE_TX_RX;
 husart3.Init.CLKPolarity = USART_POLARITY_LOW;
 husart3.Init.CLKPhase = USART_PHASE_1EDGE;
 husart3.Init.CLKLastBit = USART_LASTBIT_DISABLE;
 husart3.Init.ClockPrescaler = USART_PRESCALER_DIV1;
 husart3.SlaveMode = USART_SLAVEMODE_DISABLE;
 if (HAL_USART_Init(&husart3) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_USARTEx_SetTxFifoThreshold(&husart3, USART_TXFIFO_THRESHOLD_1_8) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_USARTEx_SetRxFifoThreshold(&husart3, USART_RXFIFO_THRESHOLD_1_8) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_USARTEx_DisableFifoMode(&husart3) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN USART3_Init 2 */

 /* USER CODE END USART3_Init 2 */

}

/**
 * @brief USB Initialization Function
 * @PAram None
 * @retval None
 */

/**
 * @brief GPIO Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_GPIO_Init(void)
{
 GPIO_InitTypeDef GPIO_InitStruct = {0};
/* USER CODE BEGIN MX_GPIO_Init_1 */
/* USER CODE END MX_GPIO_Init_1 */

 /* GPIO Ports Clock Enable */
 __HAL_RCC_GPIOC_CLK_ENABLE();
 __HAL_RCC_GPIOH_CLK_ENABLE();
 __HAL_RCC_GPIOA_CLK_ENABLE();
 __HAL_RCC_GPIOB_CLK_ENABLE();
 __HAL_RCC_GPIOD_CLK_ENABLE();

 /*Configure GPIO pin Output Level */
 HAL_GPIO_WritePin(GPIOB, ESP32_EN_Pin|LED_DRV_EN_Pin|Air_Sensor_Disable_Pin, GPIO_PIN_RESET);

 /*Configure GPIO pin Output Level */
 HAL_GPIO_WritePin(GPIOA, nCHG_TIME_EN_Pin|CHG_SOURCE_Pin, GPIO_PIN_RESET);

 /*Configure GPIO pin Output Level */
 HAL_GPIO_WritePin(GPIOC, LED2_Pin|LED1_Pin, GPIO_PIN_RESET);

 /*Configure GPIO pin : Button_Pin */
 GPIO_InitStruct.Pin = Button_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_IT_RISING_FALLING;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 HAL_GPIO_Init(Button_GPIO_Port, &GPIO_InitStruct);

 /*Configure GPIO pins : Air_INT_Pin PIR1_IN_Pin PROX1_SIG_Pin PROTO_PIR_Pin
 ACC_INT2_Pin */
 GPIO_InitStruct.Pin = Air_INT_Pin|PIR1_IN_Pin|PROX1_SIG_Pin|PROTO_PIR_Pin
 |ACC_INT2_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_IT_RISING;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);

 /*Configure GPIO pin : PROX2_SIG_Pin */
 GPIO_InitStruct.Pin = PROX2_SIG_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_IT_RISING;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 HAL_GPIO_Init(PROX2_SIG_GPIO_Port, &GPIO_InitStruct);

 /*Configure GPIO pins : ESP32_EN_Pin LED_DRV_EN_Pin Air_Sensor_Disable_Pin */
 GPIO_InitStruct.Pin = ESP32_EN_Pin|LED_DRV_EN_Pin|Air_Sensor_Disable_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);

 /*Configure GPIO pins : nCHG_TIME_EN_Pin CHG_SOURCE_Pin */
 GPIO_InitStruct.Pin = nCHG_TIME_EN_Pin|CHG_SOURCE_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);

 /*Configure GPIO pins : LED2_Pin LED1_Pin */
 GPIO_InitStruct.Pin = LED2_Pin|LED1_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);

 /*Configure GPIO pin : ACC_INT1_Pin */
 GPIO_InitStruct.Pin = ACC_INT1_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_IT_RISING;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 HAL_GPIO_Init(ACC_INT1_GPIO_Port, &GPIO_InitStruct);

 /*Configure GPIO pin : COMP_OUT_Pin */
 GPIO_InitStruct.Pin = COMP_OUT_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 HAL_GPIO_Init(COMP_OUT_GPIO_Port, &GPIO_InitStruct);

 /*Configure GPIO pin : HALL_Pin */
 GPIO_InitStruct.Pin = HALL_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_IT_FALLING;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 HAL_GPIO_Init(HALL_GPIO_Port, &GPIO_InitStruct);

 /* EXTI interrupt init*/
 HAL_NVIC_SetPriority(EXTI13_IRQn, 0, 0);
 HAL_NVIC_EnableIRQ(EXTI13_IRQn);

/* USER CODE BEGIN MX_GPIO_Init_2 */
/* USER CODE END MX_GPIO_Init_2 */
}

/* USER CODE BEGIN 4 */
void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin)
{
 if(GPIO_Pin == Button_Pin) {
 HAL_GPIO_WritePin(GPIOC, GPIO_PIN_11, GPIO_PIN_SET);

 } else {
	 HAL_GPIO_WritePin(GPIOC, GPIO_PIN_11, GPIO_PIN_RESET);
 }
}

/* USER CODE END 4 */

/**
 * @brief Period elapsed callback in non blocking mode
 * @note This function is called when TIM1 interrupt took place, inside
 * HAL_TIM_IRQHandler(). It makes a direct call to HAL_IncTick() to increment
 * a global variable "uwTick" used as application time base.
 * @PAram htim : TIM handle
 * @retval None
 */
void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim)
{
 /* USER CODE BEGIN Callback 0 */

 /* USER CODE END Callback 0 */
 if (htim->Instance == TIM1) {
 HAL_IncTick();
 }
 /* USER CODE BEGIN Callback 1 */

 /* USER CODE END Callback 1 */
}

/**
 * @brief This function is executed in case of error occurrence.
 * @retval None
 */
void Error_Handler(void)
{
 /* USER CODE BEGIN Error_Handler_Debug */
 /* User can add his own implementation to report the HAL error return state */
 __disable_irq();
 while (1)
 {
 }
 /* USER CODE END Error_Handler_Debug */
}

#ifdef USE_FULL_ASSERT
/**
 * @brief Reports the name of the source file and the source line number
 * where the assert_param error has occurred.
 * @PAram file: pointer to the source file name
 * @PAram line: assert_param error line source number
 * @retval None
 */
void assert_failed(uint8_t *file, uint32_t line)
{
 /* USER CODE BEGIN 6 */
 /* User can add his own implementation to report the file name and line number,
 ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
 /* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */

 

 

6 replies

ST Employee
August 14, 2024

Hello @Player_Saturn ,

It appears that you are enabling multiple peripherals simultaneously. I recommend enabling only the EXTI and testing it in isolation to determine if the issue persists. For your reference, you can consult the GPIO_EXTI example provided in the STM32H5 firmware package.

BRs,

 

 

"Please close this topic by clicking on “Accept as solution"" button if it fully answered your question."
Associate
August 15, 2024

Thank You for your response.

I disabled the other peripherals but still get the same result.

After entering debug mode, it does not seem to recognize the button press, however i verified it with a multimeter, and also read the pin in the main loop and it recognized the change there. 

Here is the updated code. 

/* USER CODE BEGIN Header */
/**
 ******************************************************************************
 * @file : main.c
 * @brief : Main program body
 ******************************************************************************
 * @attention
 *
 * Copyright (c) 2024 STMicroelectronics.
 * All rights reserved.
 *
 * This software is licensed under terms that can be found in the LICENSE file
 * in the root directory of this software component.
 * If no LICENSE file comes with this software, it is provided AS-IS.
 *
 ******************************************************************************
 */
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"

/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */

/* USER CODE END Includes */

/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */

/* USER CODE END PTD */

/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */

/* USER CODE END PD */

/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */

/* USER CODE END PM */

/* Private variables ---------------------------------------------------------*/

/* USER CODE BEGIN PV */

/* USER CODE END PV */

/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_SAU_Init(void);
static void MX_ICACHE_Init(void);
/* USER CODE BEGIN PFP */

/* USER CODE END PFP */

/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
uint8_t bpin = 0;
/* USER CODE END 0 */

/**
 * @brief The application entry point.
 * @retval int
 */
int main(void)
{

 /* USER CODE BEGIN 1 */

 /* USER CODE END 1 */

 /* MCU Configuration--------------------------------------------------------*/

 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();

 /* USER CODE BEGIN Init */

 /* USER CODE END Init */

 /* Configure the system clock */
 SystemClock_Config();

 /* USER CODE BEGIN SysInit */

 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_SAU_Init();
 MX_ICACHE_Init();
 /* USER CODE BEGIN 2 */

 /* USER CODE END 2 */

 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 while (1)
 {
 /* USER CODE END WHILE */

 /* USER CODE BEGIN 3 */
 }
 /* USER CODE END 3 */
}

/**
 * @brief System Clock Configuration
 * @retval None
 */
void SystemClock_Config(void)
{
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

 /** Configure the main internal regulator output voltage
 */
 __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE3);

 while(!__HAL_PWR_GET_FLAG(PWR_FLAG_VOSRDY)) {}

 /** Initializes the RCC Oscillators according to the specified parameters
 * in the RCC_OscInitTypeDef structure.
 */
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
 RCC_OscInitStruct.HSIState = RCC_HSI_ON;
 RCC_OscInitStruct.HSIDiv = RCC_HSI_DIV2;
 RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }

 /** Initializes the CPU, AHB and APB buses clocks
 */
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
 |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2
 |RCC_CLOCKTYPE_PCLK3;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSI;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
 RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
 RCC_ClkInitStruct.APB3CLKDivider = RCC_HCLK_DIV1;

 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_1) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure the programming delay
 */
 __HAL_FLASH_SET_PROGRAM_DELAY(FLASH_PROGRAMMING_DELAY_0);
}

/**
 * @brief ICACHE Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_ICACHE_Init(void)
{

 /* USER CODE BEGIN ICACHE_Init 0 */

 /* USER CODE END ICACHE_Init 0 */

 /* USER CODE BEGIN ICACHE_Init 1 */

 /* USER CODE END ICACHE_Init 1 */

 /** Enable instruction cache in 1-way (direct mapped cache)
 */
 if (HAL_ICACHE_ConfigAssociativityMode(ICACHE_1WAY) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_ICACHE_Enable() != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN ICACHE_Init 2 */

 /* USER CODE END ICACHE_Init 2 */

}

/**
 * @brief SAU Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_SAU_Init(void)
{

 /* USER CODE BEGIN SAU_Init 0 */

 /* USER CODE END SAU_Init 0 */

 /* USER CODE BEGIN SAU_Init 1 */

 /* USER CODE END SAU_Init 1 */
 /* USER CODE BEGIN SAU_Init 2 */

 /* USER CODE END SAU_Init 2 */

}

/**
 * @brief GPIO Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_GPIO_Init(void)
{
 GPIO_InitTypeDef GPIO_InitStruct = {0};
/* USER CODE BEGIN MX_GPIO_Init_1 */
/* USER CODE END MX_GPIO_Init_1 */

 /* GPIO Ports Clock Enable */
 __HAL_RCC_GPIOC_CLK_ENABLE();
 __HAL_RCC_GPIOH_CLK_ENABLE();
 __HAL_RCC_GPIOA_CLK_ENABLE();
 __HAL_RCC_GPIOB_CLK_ENABLE();

 /*Configure GPIO pin Output Level */
 HAL_GPIO_WritePin(GPIOC, LED2_Pin|LED1_Pin, GPIO_PIN_RESET);

 /*Configure GPIO pin : Button_Pin */
 GPIO_InitStruct.Pin = Button_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_IT_RISING_FALLING;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 HAL_GPIO_Init(Button_GPIO_Port, &GPIO_InitStruct);

 /*Configure GPIO pins : LED2_Pin LED1_Pin */
 GPIO_InitStruct.Pin = LED2_Pin|LED1_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);

 /* EXTI interrupt init*/
 HAL_NVIC_SetPriority(EXTI13_IRQn, 0, 0);
 HAL_NVIC_EnableIRQ(EXTI13_IRQn);

/* USER CODE BEGIN MX_GPIO_Init_2 */
/* USER CODE END MX_GPIO_Init_2 */
}

/* USER CODE BEGIN 4 */
void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin)
{
 if(GPIO_Pin == GPIO_PIN_13) {
 HAL_GPIO_WritePin(GPIOC, GPIO_PIN_11, GPIO_PIN_SET);

 } else {
	 HAL_GPIO_WritePin(GPIOC, GPIO_PIN_11, GPIO_PIN_RESET);
 }
}

/* USER CODE END 4 */

/**
 * @brief Period elapsed callback in non blocking mode
 * @note This function is called when TIM1 interrupt took place, inside
 * HAL_TIM_IRQHandler(). It makes a direct call to HAL_IncTick() to increment
 * a global variable "uwTick" used as application time base.
 * @PAram htim : TIM handle
 * @retval None
 */
void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim)
{
 /* USER CODE BEGIN Callback 0 */

 /* USER CODE END Callback 0 */
 if (htim->Instance == TIM1) {
 HAL_IncTick();
 }
 /* USER CODE BEGIN Callback 1 */

 /* USER CODE END Callback 1 */
}

/**
 * @brief This function is executed in case of error occurrence.
 * @retval None
 */
void Error_Handler(void)
{
 /* USER CODE BEGIN Error_Handler_Debug */
 /* User can add his own implementation to report the HAL error return state */
 __disable_irq();
 while (1)
 {
 }
 /* USER CODE END Error_Handler_Debug */
}

#ifdef USE_FULL_ASSERT
/**
 * @brief Reports the name of the source file and the source line number
 * where the assert_param error has occurred.
 * @PAram file: pointer to the source file name
 * @PAram line: assert_param error line source number
 * @retval None
 */
void assert_failed(uint8_t *file, uint32_t line)
{
 /* USER CODE BEGIN 6 */
 /* User can add his own implementation to report the file name and line number,
 ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
 /* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */

 

ST Employee
August 15, 2024

Hello @Player_Saturn ,

Your settings should be okay, could you pls check whether the EXTI13_IRQHandler function in your stm32h5xx_it.c file is executed when you press the button?

If it is not, could you please specify the board you are working with so that I can check on my end?

 

Best Regards,

"Please close this topic by clicking on “Accept as solution"" button if it fully answered your question."
Visitor
June 25, 2026

I had the same problem with the STM32H523CEt6. But I managed to get it to work now.

Just make sure that the interrupt priority is set to a number greater than 0. Check that you either have pull-up or pull down resister on that pin (i.e. in the GPIO) section. Make sure EXTI LINE INTERRUPT is checked (i.e. GPIO in the NVIC tab). Once the code is generated,  write your code in the interrupt handler in the _it.c file. It seems that write your code in the callback function just won't work. Please try this and let me know if it still not firing. Note: I only have STM32H523Cet6 though,  but it works now 

 

Richard Li
Senior
June 25, 2026

There is Copilot pointed, you didn’t create IRQHandle.

 

 IRQ handler → call HAL_GPIO_EXTI_IRQHandler()

This goes in stm32f1xx_it.c:

 

void EXTI0_IRQHandler(void)
{
HAL_GPIO_EXTI_IRQHandler(GPIO_PIN_0);
}

This is mandatory — the HAL does not call your callback unless this function is invoked.

Visitor
June 25, 2026

That is is actually there and work well for the F4 MCU, but for the H523CET6 I had to write everything in the interrupt handler, because it does not called the callback function. These STM32H523CET have a lot of things that just don’t work correctly,  one will need to play around with a number of part just to get it to work.

I have used STM32F03, STM32F7, STM32F1 blue pill, STM32F4 and even STM32H7, I have never seen such behavior like that I am seeing with the  STM32H523CET. Because with the STM32H523CET even a simple thing like USB-CDC is just doesn’t work. I could not get the UART modules to work, but I finally got them right.

There was a time when I though I should just through them away, but mmmmh…

I just hope STM look into this MCU (i.e. STM32H523CET) again and maybe update the package to make them user friendly.