Skip to main content
Associate
Sep 11, 2025 8:41 AM UTC
Question

STM32G474RE CRC feed from buffer via DMA memory transfer.

I want to use the standalone CRC module to offload calculations AND transfers from CPU - using purely DMA memory transfers - is this possible on the STM32G474RE?

This topic has been closed for replies.

1 reply

ST Technical Moderator
Sep 11, 2025 10:20 AM UTC

Hello @Spam4tea 

Yes, it is possible to use DMA to offload CRC calculations on the STM32G474RE

Please refer to the AN4187 for more details. 

The recommended steps are as follows:

  1. Configure CRC module.
  2. Configure DMA.
  3. Start DMA transfer.
  4. Wait for DMA transfer complete interrupt/flag.
  5. In the complete callback function read CRC result from CRC->DR.

 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om