Skip to main content
Associate II
Nov 15, 2025 8:01 PM UTC
Solved

STM32G4 Dual Injected Simultaneous Mode ADC2 Returns 0

I'm using STM32G474 with dual ADC injected simultaneous mode. İndividual ADC injected mode works ok.

ADC1 is triggered by TIM1 Channel 4 and the interrupt is firing correctly, but ADC2 always returns zero.

 

Questions:

  1. Why does ADC2->JDR1 always return 0 in dual injected simultaneous mode?
  2. Is it correct that HAL_ADCEx_InjectedStart_IT(&hadc2) returns HAL_ERROR in dual mode?

You can see my ADC1 and ADC2 configuration.

void HAL_ADCEx_InjectedConvCpltCallback(ADC_HandleTypeDef* hadc)
{
 if (hadc->Instance == ADC1) {

 	HAL_GPIO_WritePin(GPIOA, GPIO_PIN_4, GPIO_PIN_SET);
 	HAL_GPIO_WritePin(GPIOA, GPIO_PIN_4, GPIO_PIN_RESET);

 adc1 = ADC1->JDR1;

 adc2 = ADC2->JDR1;
 }

}

 

static void MX_ADC1_Init(void)
{

 /* USER CODE BEGIN ADC1_Init 0 */

 /* USER CODE END ADC1_Init 0 */

 ADC_MultiModeTypeDef multimode = {0};
 ADC_InjectionConfTypeDef sConfigInjected = {0};
 ADC_ChannelConfTypeDef sConfig = {0};

 /* USER CODE BEGIN ADC1_Init 1 */

 /* USER CODE END ADC1_Init 1 */

 /** Common config
 */
 hadc1.Instance = ADC1;
 hadc1.Init.ClockPrescaler = ADC_CLOCK_SYNC_PCLK_DIV4;
 hadc1.Init.Resolution = ADC_RESOLUTION_12B;
 hadc1.Init.DataAlign = ADC_DATAALIGN_RIGHT;
 hadc1.Init.GainCompensation = 0;
 hadc1.Init.ScanConvMode = ADC_SCAN_DISABLE;
 hadc1.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
 hadc1.Init.LowPowerAutoWait = DISABLE;
 hadc1.Init.ContinuousConvMode = DISABLE;
 hadc1.Init.NbrOfConversion = 1;
 hadc1.Init.DiscontinuousConvMode = DISABLE;
 hadc1.Init.ExternalTrigConv = ADC_SOFTWARE_START;
 hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;
 hadc1.Init.DMAContinuousRequests = DISABLE;
 hadc1.Init.Overrun = ADC_OVR_DATA_PRESERVED;
 hadc1.Init.OversamplingMode = DISABLE;
 if (HAL_ADC_Init(&hadc1) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure the ADC multi-mode
 */
 multimode.Mode = ADC_DUALMODE_INJECSIMULT;
 multimode.DMAAccessMode = ADC_DMAACCESSMODE_DISABLED;
 multimode.TwoSamplingDelay = ADC_TWOSAMPLINGDELAY_1CYCLE;
 if (HAL_ADCEx_MultiModeConfigChannel(&hadc1, &multimode) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure Injected Channel
 */
 sConfigInjected.InjectedChannel = ADC_CHANNEL_2;
 sConfigInjected.InjectedRank = ADC_INJECTED_RANK_1;
 sConfigInjected.InjectedSamplingTime = ADC_SAMPLETIME_2CYCLES_5;
 sConfigInjected.InjectedSingleDiff = ADC_SINGLE_ENDED;
 sConfigInjected.InjectedOffsetNumber = ADC_OFFSET_NONE;
 sConfigInjected.InjectedOffset = 0;
 sConfigInjected.InjectedNbrOfConversion = 1;
 sConfigInjected.InjectedDiscontinuousConvMode = DISABLE;
 sConfigInjected.AutoInjectedConv = DISABLE;
 sConfigInjected.QueueInjectedContext = DISABLE;
 sConfigInjected.ExternalTrigInjecConv = ADC_EXTERNALTRIGINJEC_T1_CC4;
 sConfigInjected.ExternalTrigInjecConvEdge = ADC_EXTERNALTRIGINJECCONV_EDGE_RISING;
 sConfigInjected.InjecOversamplingMode = DISABLE;
 if (HAL_ADCEx_InjectedConfigChannel(&hadc1, &sConfigInjected) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure Regular Channel
 */
 sConfig.Channel = ADC_CHANNEL_2;
 sConfig.Rank = ADC_REGULAR_RANK_1;
 sConfig.SamplingTime = ADC_SAMPLETIME_2CYCLES_5;
 sConfig.SingleDiff = ADC_SINGLE_ENDED;
 sConfig.OffsetNumber = ADC_OFFSET_NONE;
 sConfig.Offset = 0;
 if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN ADC1_Init 2 */

 /* USER CODE END ADC1_Init 2 */

}

/**
 * @brief ADC2 Initialization Function
 * None
 * @retval None
 */
static void MX_ADC2_Init(void)
{

 /* USER CODE BEGIN ADC2_Init 0 */

 /* USER CODE END ADC2_Init 0 */

 ADC_InjectionConfTypeDef sConfigInjected = {0};

 /* USER CODE BEGIN ADC2_Init 1 */

 /* USER CODE END ADC2_Init 1 */

 /** Common config
 */
 hadc2.Instance = ADC2;
 hadc2.Init.ClockPrescaler = ADC_CLOCK_SYNC_PCLK_DIV4;
 hadc2.Init.Resolution = ADC_RESOLUTION_12B;
 hadc2.Init.DataAlign = ADC_DATAALIGN_RIGHT;
 hadc2.Init.GainCompensation = 0;
 hadc2.Init.ScanConvMode = ADC_SCAN_DISABLE;
 hadc2.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
 hadc2.Init.LowPowerAutoWait = DISABLE;
 hadc2.Init.ContinuousConvMode = DISABLE;
 hadc2.Init.NbrOfConversion = 1;
 hadc2.Init.DiscontinuousConvMode = DISABLE;
 hadc2.Init.DMAContinuousRequests = DISABLE;
 hadc2.Init.Overrun = ADC_OVR_DATA_PRESERVED;
 hadc2.Init.OversamplingMode = DISABLE;
 if (HAL_ADC_Init(&hadc2) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure Injected Channel
 */
 sConfigInjected.InjectedChannel = ADC_CHANNEL_9;
 sConfigInjected.InjectedRank = ADC_INJECTED_RANK_1;
 sConfigInjected.InjectedSamplingTime = ADC_SAMPLETIME_2CYCLES_5;
 sConfigInjected.InjectedSingleDiff = ADC_SINGLE_ENDED;
 sConfigInjected.InjectedOffsetNumber = ADC_OFFSET_NONE;
 sConfigInjected.InjectedOffset = 0;
 sConfigInjected.InjectedNbrOfConversion = 1;
 sConfigInjected.InjectedDiscontinuousConvMode = DISABLE;
 sConfigInjected.AutoInjectedConv = DISABLE;
 sConfigInjected.QueueInjectedContext = DISABLE;
 sConfigInjected.InjecOversamplingMode = DISABLE;
 if (HAL_ADCEx_InjectedConfigChannel(&hadc2, &sConfigInjected) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN ADC2_Init 2 */

 /* USER CODE END ADC2_Init 2 */

}

 

Saket_OmBest answer
ST Technical Moderator
Nov 19, 2025 1:08 PM UTC

Hello @batuhanky 

In your case ADC2 should be started before ADC1.  

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om

1 reply

Saket_OmBest answer
ST Technical Moderator
Nov 19, 2025 1:08 PM UTC

Hello @batuhanky 

In your case ADC2 should be started before ADC1.  

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om