Skip to main content
New.Fish
Associate III
Jul 19, 2021 2:16 AM UTC
Question

STM32G0 USB_DP/DM 3.3Volt

we are planning to use STM32G0 for our next generation design with its USB port, two application is considered:

  1. Use it as VCP, the signal from PC is +5 Volt, but the MCU is +3.3 Volt, can the USB port DP/DM pin directly connect to MCU pins? or require 5 V to 3.3 Volt converter?
  2. Use as a Mas storage class, connect to USB drive to read/write files. USB works with 5 Volt power, can USB work with 3.3 Volt power supply? if YES, then USB and MCU can share same power supply. Otherwise we will have another 5 Volt power on board which will introduce extra cost.

This topic has been closed for replies.

2 replies

waclawek.jan
Super User
Jul 19, 2021 2:46 AM UTC

DM/DP signals are 3V, no level conversion needed.

VBUS is 5V, you have to supply it to USB device if you want to use the STM32 as Host.

JW

New.Fish
New.FishAuthor
Associate III
Jul 19, 2021 3:04 AM UTC

Thanks.

Is there any examples code about how to use VCP?