Skip to main content
DRobe.4
Associate III
May 3, 2023 4:44 AM UTC
Solved

STM32G0 USART3 and USART4 share an interrupt. How to deal with it?

void USART3_IRQHandler(void) is incorrect, since USARTs 3/4 share the interrupt, it doesn't compile. What replaces 'USART3' in the interrupt handler?

NVIC_ClearPendingIRQ(USART3_IRQn); is incorrect since USART3 3/4 share the interrupt. What replaces 'USART3_IRQn' so that the NVIC_ClearPendingIRQ will compile?

This topic has been closed for replies.
KnarfB
KnarfBBest answer
Super User
May 3, 2023 5:30 AM UTC

The interrupt handler names are defined in the startup code, like in startup_stm32g070xx.s:

.word USART1_IRQHandler /* USART1 */
.word USART2_IRQHandler /* USART2 */
.word USART3_4_IRQHandler /* USART3, USART4 */

If you create code with UART 3/4 interrupts enabled, you find the code in stm32g0xx_hal_msp.c:

HAL_NVIC_SetPriority(USART3_4_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(USART3_4_IRQn);

Those defines are from CMSIS like stm32g070xx.h.

The generated code is correct and does compile without errors.

hth

KnarfB

4 replies

Tesla DeLorean
Guru
May 3, 2023 5:28 AM UTC

You check and service both peripherals and the flags should clear.

I​ think in one of the recent threads it establishes the combined symbol and number for the IRQ. Grep the library source or truncate the Handler name seen in startup.s

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Tesla DeLorean
Guru
May 3, 2023 5:30 AM UTC

YOUR thread here ​https://community.st.com/s/question/0D53W00002FEy7wSAD/i-there-a-usart3irqn-and-a-usart4irqn-on-stm32g070

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
KnarfB
KnarfBBest answer
Super User
May 3, 2023 5:30 AM UTC

The interrupt handler names are defined in the startup code, like in startup_stm32g070xx.s:

.word USART1_IRQHandler /* USART1 */
.word USART2_IRQHandler /* USART2 */
.word USART3_4_IRQHandler /* USART3, USART4 */

If you create code with UART 3/4 interrupts enabled, you find the code in stm32g0xx_hal_msp.c:

HAL_NVIC_SetPriority(USART3_4_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(USART3_4_IRQn);

Those defines are from CMSIS like stm32g070xx.h.

The generated code is correct and does compile without errors.

hth

KnarfB

DRobe.4
DRobe.4Author
Associate III
May 4, 2023 3:03 PM UTC

Everyone, thanks for your help... compiles, so I presume that it will work.